STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Open Bootloader USB I/Fbug

In attempting to figure out how to stay in the bootloader loop while exchanging packets with the USB DFU tool I came across as what looks like an unintentionally undeleted line of code.Here is the code:static void OPENBL_USART_Go(void) { uint32_t a...

Resolved! Confusion on DMAMUX registers in RM0468

     Hallo everyone,Since some time I struggle to get DMA access working on a STM32H723. I was pointed out this MCU is a complicated beast, but I would at least expect sensible, coherent documentation for it.When I look at page 683, I see:on next pag...

Screenshot_Header_DMAMUX1_CxCR.png Screenshot_Header_DMAMUX2_CxCR.png Screenshot_Header_DMAMUX_RegisterMap.png Screenshot_RM0468_Bottom_P672.png
FredS by Senior
  • 4177 Views
  • 12 replies
  • 1 kudos

Resolved! H733: MCO output active without GPIO init

Heyho,so I was just checking the MCO1 output of my STM32H733ZGT6 and found some super jittery 64 MHz with full swing between 0V and 3.3V.Then checked my code and found that I had not set the RCC->CFGR and not even initialized the GPIO.When I actually...

LCE by Principal II
  • 5480 Views
  • 13 replies
  • 2 kudos

Resolved! STM32H5 - ADC DMA - Standard Request Example

HelloI am looking for an example to get the ADC regular sequence transferred by DMA to memory going.I use TIM15 to trigger the ADC regular sequence, which has four measurements, every 5 milliseconds. When I activate the EOS IRQ and toggle a GPIO I se...

IGärt.1 by Associate II
  • 4759 Views
  • 2 replies
  • 0 kudos

PWM sine gen two timers idea

Hi, req is generate sine wave and manage frequency precisely . My design require range 2Hz to 10Hz with for example step 0,002Hz.My idea is one PWM timer for sine with same table for exampel 10bit. Second linked timer for manage one sample time on PW...

MM..1 by Chief III
  • 1194 Views
  • 2 replies
  • 0 kudos

Resolved! Enable/ disable EXTI interrupts using HAL

Hey guys.I need to enable/disable the line 14 of the EXTI interrupts multiple times, using HALDo i just use the HAL_NVIC_DisableIRQ  HAL_NVIC_EnableIRQ  ( and HAL_NVIC_SetPriority whenever i re-enable the line?), providing the correct handle to the a...

STM32H7 ADC Triggered by timer at high frequency.

Hello everyone.I am having trouble reaching the desired conversion frequency when attempting to have the ADC convert samples at a frequency of 384kHz( T ~ 2.6us ). The issue I've come across is that on each timer update signal, the ADC first has a wi...

StefanTM by Associate
  • 1236 Views
  • 1 replies
  • 0 kudos