User Activity

Hi allI'm configuring STM32U5A5VJT to work with the USB HS crystaless. From the Cube it seems to be possibile to use one of the integrated oscillators as clock source for the USB HS but this is not mentioned in the datasheet.I'm afraid that it could ...
Posted on April 22, 2018 at 09:03Hi alli want to use Hyperram on STM32H7. It has got QuadSPI while Hyperram is designed to work with the OctoSPI present on STM32L4+. Can I use the dual QuadSPI to emulate the OctoSPI?Ivano
Posted on March 24, 2016 at 11:35Hi allI'm using the USB microphone example on STM32L4 nucleo board ad I've modified the source code to adapt the buffer dimention according to the synchronization of the PC request and data coming from the SAI connec...