STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Dead Band issue with HRTIM module.

Dear team,I am using a STM32G474 in my application. I've generated a PWM in the HRTIM TIMER E that is active low (necessary for the requirements of the modulation). I want to insert a dead band between this signal and its complementary (Output 2). Th...

Captura.PNG
PMoreno by Associate II
  • 2235 Views
  • 2 replies
  • 0 kudos

Resolved! STSW-LINK009 Software ZIP file

Hello, ST community, I am having trouble installing a Batch file from the STSW-LINK009 Software ZIP file. I am on a Macbook Pro M2, running Parallels Windows 11. When I try to download the "stlink_winusb_install" batch file I get a pop-up saying that...

64-Bit Verison POP-UP.png
alan29 by Associate
  • 2744 Views
  • 3 replies
  • 0 kudos

I2C errors handling in EFT

 Hi,I am working with stm32g491re.I am communicating with TCA9537(Ioexpander) from stm32 through I2C. It will control a realy. For my product EFT(Electrical Fast Transient) testing, After starting EFT teat relay getting turned off and not recovering....

sireevenkat1_0-1724937646761.png

STM32H743 RTC Clock configuration failure

Hello, I'm working on STM32H743BIT6, It is in production phase. During flashing the software, it is failed to configure LSE crystal with internal RTC enabled. out of 50 boards 2 board got failed.During debug it is observed that the RTC clock configur...

SPI between mcu

@Erwan SZYMANSKI I am trying to establish SPI communication between two STM boards: the Nucleo G431RB as the master and the STM32MP157F-DK2 as the slave. I followed the instructions provided in the Getting Started with SPI guide and configured the se...

nesnes by Associate III
  • 1329 Views
  • 0 replies
  • 0 kudos

Use MOSFETS with STM32 to power up sensors

Hello everyone! I want to use some MOSFETS to individually power up/down sensors on a PCB. Here's the schematics :  The MOSFET is a DMG1012T-7 (N-Channel) and here's it's datasheet : https://www.lcsc.com/datasheet/lcsc_datasheet_1809050424_Diodes-Inc...

yaxsomo_0-1725350654452.png
yaxsomo by Associate III
  • 2096 Views
  • 1 replies
  • 0 kudos

Resolved! CAN Write State issue

Dear, I am trying to run the CAN Communication in STM32F407 discovery board, In CAN_INIT I have made controller state to Ready after that I have changed the controller state from ready to LISTENING in CAN_START function,   but when I am trying to exe...