while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ HAL_ADC_Start(&hadc2); HAL_ADC_Start(&hadc1); if (HAL_ADC_PollForConversion(&hadc2, 10) == HAL_OK) { adcValTemp = HAL_ADC_GetValue(&hadc2); // Temperature Calculation adcTem...
Hello I have another question
I am currently working on a microcontroller project I am building a GPS tachometer which transfers the NMEA data of the GNSS 4 Click Module from Mikroe via UART to my STM32L052K6T6 and outputs it to a display
How c...
HelloI am currently working on a microcontroller project I am building a GPS tachometer which transfers the NMEA data of the GNSS 4 Click Module from Mikroe via UART to my STM32L052K6T6 and outputs it to a displayI have so far UART initialized with t...
here i also go the c# code public partial class Form1 : Form { string inbuffer; public Form1() { InitializeComponent(); serialPort1.Open(); } private void DisplayText(object sender, EventArgs e) { label1.Text = Conv...