STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! OTG_HPRT>PENCHNG bit in STM32H743

[Not a bug report, explanation below, first post kept for context]I'm writing a USB host library for the STM32H743 rev V. Bits PENA and PENCHNG of register OTG_HPRT represent Port enable and Port enable/disable change. Port enable is supposed to be a...

JBernard_1-1725316374583.png JBernard_2-1725316381451.png lS9ZB1H.png K831E2a.png
JBernard by Associate II
  • 1814 Views
  • 2 replies
  • 1 kudos

Repetition Timer PWM Help

 Hello, I'm wondering if there is an obvious way to generate a limited set of n pulses from an external trigger?At the moment i'm using TIM8 in one pulse mode with repetition but my problem is that i want the White pulse train to start with the risin...

Stemcy_0-1725299151951.png
Stemcy by Associate
  • 2123 Views
  • 4 replies
  • 4 kudos

Resolved! NRST Pin going low while programming for a milli second.

Hii,I am working with stm32f100 series microcontroller, where I am having issue with NRST pin, I have connected a capacitor of 0.1uF(also tried 10uF) between NRST pin and ground. Microcontroller has an internal pullup. and it is showing 3.3V at the t...

image.png
Ragini by Associate II
  • 2438 Views
  • 5 replies
  • 0 kudos

STM32H7 Custom Project Schematic review help

Hi guys,I been working on this project for some time now on my "free time"...but so far without any success.In the first prototype I have assembled all the peripherals(QSPI, eMMC, SDRAM, some I2C and SPI slaves peripherals and DSI display.).Nothing s...

pema_0-1724698352193.png pema_1-1724698368494.png pema_2-1724698389561.png pema_3-1724698407578.png
pema by Associate II
  • 3071 Views
  • 5 replies
  • 4 kudos

DMA channel1 Stream 0-7 which channel to choose

Hi i m working on H732 timer1 as PWM and its working fine, but when I try to implement DMA on timer1, there is no waveform. I enclosed the DMA code below, as I declare an array of 10 PWM duty cycle values..i suspect it's the Timer1 channel1 stream th...

StanJerm_0-1725327735894.png
StanJerm by Associate III
  • 3112 Views
  • 6 replies
  • 0 kudos

Resolved! HardFault when using UART and DMA

Hi, I have a program running on a STM32U083RCT that is raising a HardFault when running at full speed, but when stepping through the code using a debugger the code appears to run correctly. I have a transceiver device connected to to USART2. I have a...

Jorgie by Associate III
  • 2054 Views
  • 2 replies
  • 0 kudos

Lora Basics Modem on STM32L073RZT6

Hello, I'm working on testing the LoRa Basics Modem V4, available in SWL2001 on github, and for now I've managed to generate the executable and download the program on the board I have, but nothing has appeared yet on The Things Network. I believe th...

stm32 GPIO input from mcp23017 interrupt

Hello,I'm working on a project involving an STM32F103 and a mcp23017 port expander.I've connected the mcp23017 INTA to PA15, no pull-up or down involved.I'm able to drive the mcp23017 via I2C, no problem about that.The problem I have is detecting the...