User Activity

Hi,I am using an STM32H7 TIM8 unit to generate a PWM signal with a fixed number of pulses.  The TIM unit is configured in one-shot mode and the repetition counter is configured to generate the desired number of pulses, after which the timer automatic...
I am trying to use the PLL1 fractional PLL on a Nucleo-U545RE-Q board to fine-tune a frequency measurement.  RM0456 rev 5 has the following procedure to adjust the fractional PLL:"If the application intends to tune the PLLx frequency on-the-fly, then...
Hello,I was trying to implement extended calibration for ADC1 on my STM32U575 according to RM0456 Rev 5.  I have a revision ID 0x3001 chip which should support extended calibration.  The chip would hang very badly (can no longer connect with debug pr...
Hello,We are using the STM32C0 in a low-power application.  We initially selected the part with 12K SRAM in case we needed to use more than 6K, but after development have found that we can make do with 6K.  I am curious if there is any power savings ...
Hello,In STM32C0 RM0490, section 5.4.16, the RCC_AHBSMENR describes the bit SRAMSMEN which can be used to disable the SRAM clock during Sleep mode to save power.  We will be using the STM32C0 in a low-power application and I was wondering if the SRAM...
Kudos from