STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB-HS without ULPI-PHY

Hi,We are using the STM32F446RCT6TR together with a ULPI-PHY in an application to be able to use USB-HS. Is there a controller from ST with which we can dispense with the ULPI-PHY if we use USB-HS + USB-FS with otherwise the same properties as the ST...

TR01 by Associate
  • 2119 Views
  • 5 replies
  • 4 kudos

STM32C0xx BOOT0 PIN Legacy mode

Good morning,We designed a LED controller with the STM32C011. We exposed the BOOT0 PIN in our design as followed: Now the first prototypes are potted in without access to the SWD interface and we want to update the firmware via the internal bootloade...

NickvanIJzendoorn_0-1727941798010.png NickvanIJzendoorn_2-1727942358582.png NickvanIJzendoorn_1-1727942193724.png

Time Delay in FFT performance

Hello community,The CMSIS DSP library supports a 4096-point FFT, but my project requires a 16384-point FFT. I added some extra library files (downloaded from GitHub; these files are written in C) to my project and successfullyperformed a 16384-point ...

SA  V.1 by Senior
  • 7099 Views
  • 14 replies
  • 5 kudos

Resolved! STM32U5F9NJ FDCAN Peripheral Not Initializing

Hello,I'm having problems implementing the FDCAN peripheral on the STM32U5F9 TFBGA-216 package. The peripheral is present and configurable in the IDE, but none of the registers update during initialization. In addition to my code, I've tried a bare p...

dhein by Associate
  • 1980 Views
  • 4 replies
  • 2 kudos

How to write data efficiently to an SD card ?

I am writing data to an SD card for a data logger application, but I have very little experience with writing to SD cards so I want to ensure I am writing the data efficiently.My understanding is that data is written as a sector of 512 bytes.  So eve...

johngj_2-1707419795099.png johngj_3-1707421018110.png
johngj by Senior
  • 21814 Views
  • 11 replies
  • 8 kudos

Resolved! STM32F103RB AF bit of I2C1_SR1 don't work

Hello,STM32F103RB microcontroller.7-bit master transmitter (see Figure 273).When I send Address then I receive AF bit of I2C_SR1 register equals "1" (Acknowledge failure). But the diagram taken from the oscilloscope shows that after the address there...

Mykola_Levun_1-1726487576667.png

Resolved! STM32H745: USB MSC stuck at configASSERT

Hello :)I have created a project for a STM32H745I_Disco board in TouchGFX, imported it to STM32CubeIDE and enabled:USB_OTG_FS -- Host_Only and VBUS sensingUSB_HOST_M7 -- Mass Storage Host Class + Platform settings for enable PinFATFS_M7 -- USB Disk, ...

FabianEbs by Associate III
  • 3101 Views
  • 4 replies
  • 2 kudos