STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! External 24bit DAC interface with nucleo board

I need to generate the millivolts of range between (-10mv to 100mv) with three decimal point accuracy using 24-bit external DAC interfaced with NUCLEO-L496ZG board. Is it possible to generate the range?I need HeadsUp & suggestion to achieve the menti...

akash07 by Associate II
  • 3385 Views
  • 6 replies
  • 3 kudos

Resolved! stm32f103re CRC ?

 hi i used of CRC in stm32CubeMX and for check true worked CRC used of two online CRC calculator site:https://www.sunshine2k.de/coding/javascript/crc/crc_js.html&https://crccalc.com/?crc=123456789&method=&datatype=0&outtype=0 i think stm32cubeIDE int...

kshin.111 by Associate III
  • 2970 Views
  • 6 replies
  • 7 kudos

OSPI Clock Configuration on STM32U5A9J-DK

Hi, I am currently working on configuring the OSPI clock for the STM32U5A9J-DK board, and I have some questions regarding the configuration. From my understanding, based on the Clock Configuration tab in the STM32CubeIDE (.ioc file), the clock going ...

sohm by Associate III
  • 2310 Views
  • 2 replies
  • 1 kudos

DMA latency

I working through issues on an STM32G4 where at times I'm not getting the reaction time from the DMA that I would like. I read AN2548, and it is a very helpful resource. However, I'm seeing slightly worse response times than AN2548 would suggest, and...

tek00077.png tek00076.png
Lee3 by Associate III
  • 2404 Views
  • 2 replies
  • 0 kudos

How to store data in flash memory of STM32F401CCU6?

My STM32F401CCU6 has 256K flash memory, and I want to use it to store some data. Trying to create a user kept pausing the program at the hardfault handler when I tried debugging. Where am I going wrong? Are there any good resources for this microcont...

MihirJ by Associate II
  • 1775 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H753VITx with ULPI USB3320 - corrupted data?

 Dear all,for the past few weeeks, I've been trying to get the STM32H753VIT6 up and running with the USB3320 ULPI interface but I have not been succesfull. First, I have tried to run a CubeMX generated USB CDC example to test the functionality, but t...

ulpi_read_reg_0x00.png vosahlov_0-1727957108920.png
vosahlov by Associate II
  • 5183 Views
  • 3 replies
  • 3 kudos