STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash via I2C bootloader problem for STM32G0B1CEU6

Hello,I encountered a problem with the internal Bootloader of the STM32G0B1CEU6 MCU.ConditionsFirst, the option bytes are set with an STLINK-V3 programming adapter (SWD interface) and CubeProgrammer (2.15.0) according to Pattern 11 of AN2606:nBoot_SE...

abasty by Associate
  • 1084 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 Nucleo Continuous ADC mode only converts once

Hello Forum,I have an issue performing continuous conversions with the ADC on my STM Nucleo board. I want to continuously convert once the ADC is initialized and started and do something with the data afterwards (what is irrelevant to the problem). H...

Resolved! Unable to read stepsize of DAC

I have configured DAC in nucleol496zg board using an internal voltage reference of scale around 2.048V , it is 12 bit DAC so step size would be around 0.5mv but when i write HAL_DAC_Start(&hdac1,DAC_CHANNEL_1); HAL_DAC_SetValue(&hdac1, DAC_CHANNEL...

akash07 by Associate II
  • 1006 Views
  • 1 replies
  • 0 kudos

Inverted DAC output

Posted on May 30, 2014 at 17:16Any ideas what would cause a STM32F4 Discovery board to suddenly invert the DAC output, such that 0 gives 3V and 4095 gives 0V? This does not seem to be a programming issue as the identical program worked fine prior (a...

bridges by Associate II
  • 1751 Views
  • 2 replies
  • 0 kudos

STM32H573 I2S audio clock problem

Hi, I'm trying to set the following parameters for I2S in Device Configuration Tool (STM32CubeIDE v1.14.0): - Master Clock Output enable - audio frequency: 48kHz - Data and Frame Format: 16 bits I want to connect an external 12.288 MHz clock to the A...

Wojtek2 by Associate
  • 3730 Views
  • 4 replies
  • 0 kudos

Resolved! Questions about saving data to flash

I am working with an STM32D103C8T6 and I want to store some data on the flash memory.I have some idea on how to do It but not sure about some details.My procedure is the following:1- Add a new section in linker at a defined address near the end.I und...

STM32U5A9 GPDMA unusable data with MDF

Hi, I'm trying to use AMC1336 Delta-Sigma Modulator with STM32U5A9 MDF. I have tried using polling and interrupts for data acquisition and got expected results. But when I tried switching to GPDMA the data jumped around and is not usable. I took 100 ...

IT_dc.PNG DMA_dc.PNG GPDMA_config.PNG MDF_config.PNG