Skip to main content
Associate
May 26, 2024
Solved

FDCAN on Riverdi LCD not send and not received - STM32H757XIH6

  • May 26, 2024
  • 1 reply
  • 1273 views

Hi all,

For several days I have been trying to send and receive something via CAN, but I am unable to do so on the Riverdi LCD board. I read two posts here with similar problems and instructions and videos from ST, but it did not solve my problem. CAN still does not work in normal mode. I tried too on loopback mode

STM board: >>  Riverdi board

 On the second board with nucleo 64, I made a simple program that sends 8 bytes and works correctly.

nucleo.jpg

But riverdi board send like this

riverdi.jpg

Now FDCAN set is to 40Mhz and this is code fdcan.c:

 

 

 

 

 

void MX_FDCAN1_Init(void)
{
 hfdcan1.Instance = FDCAN1;
 //hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_NO_BRS;
 //hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK; //I try too
 hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan1.Init.AutoRetransmission = ENABLE;
 hfdcan1.Init.TransmitPause = DISABLE;
 hfdcan1.Init.ProtocolException = DISABLE;
 hfdcan1.Init.NominalPrescaler = 1;
 hfdcan1.Init.NominalSyncJumpWidth = 10; //ok
 hfdcan1.Init.NominalTimeSeg1 = 69;
 hfdcan1.Init.NominalTimeSeg2 = 10;
 hfdcan1.Init.DataPrescaler = 20; //ok
 hfdcan1.Init.DataSyncJumpWidth = 1; //ok
 hfdcan1.Init.DataTimeSeg1 = 2; //ok
 hfdcan1.Init.DataTimeSeg2 = 1; //ok
 hfdcan1.Init.MessageRAMOffset = 0;
 hfdcan1.Init.StdFiltersNbr = 1;
 hfdcan1.Init.ExtFiltersNbr = 0;
 hfdcan1.Init.RxFifo0ElmtsNbr = 1; //ok
 hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.RxFifo1ElmtsNbr = 0;
 hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.RxBuffersNbr = 0;
 hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.TxEventsNbr = 0;
 hfdcan1.Init.TxBuffersNbr = 0;
 hfdcan1.Init.TxFifoQueueElmtsNbr = 1; //ok
 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;

 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }
 FDCAN_FilterTypeDef canfilterconfig;

 canfilterconfig.IdType = FDCAN_STANDARD_ID;
 canfilterconfig.FilterIndex = 0;
 canfilterconfig.FilterType = FDCAN_FILTER_MASK; //FDCAN_FILTER_RANGE
 canfilterconfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
 canfilterconfig.FilterID1 = 0x100;
 canfilterconfig.FilterID2 = 0x100;
 canfilterconfig.RxBufferIndex = 0;

 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &canfilterconfig) != HAL_OK)
 {
 /* Filter configuration Error */
 Error_Handler();
 }

 HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);

}

void HAL_FDCAN_MspInit(FDCAN_HandleTypeDef* fdcanHandle)
{

 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(fdcanHandle->Instance==FDCAN1)
 {
 /* USER CODE BEGIN FDCAN1_MspInit 0 */

 /* USER CODE END FDCAN1_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_FDCAN;
 PeriphClkInitStruct.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* FDCAN1 clock enable */
 HAL_RCC_FDCAN_CLK_ENABLED++;
 if(HAL_RCC_FDCAN_CLK_ENABLED==1){
 __HAL_RCC_FDCAN_CLK_ENABLE();
 }

 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**FDCAN1 GPIO Configuration
 PB9 ------> FDCAN1_TX
 PA11 ------> FDCAN1_RX
 */
 GPIO_InitStruct.Pin = GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_11;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* FDCAN1 interrupt Init */
 HAL_NVIC_SetPriority(FDCAN1_IT0_IRQn, 5, 0);
 HAL_NVIC_EnableIRQ(FDCAN1_IT0_IRQn);

 /* USER CODE BEGIN FDCAN1_MspInit 1 */

 /* USER CODE END FDCAN1_MspInit 1 */
 }
}

 

 

 

 

 

And program code:

 

 

 

 

 

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "quadspi.h"
#include "myfile.h"
#include "max31855.h"

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

#ifndef HSEM_ID_0
#define HSEM_ID_0 (0U) /* HW semaphore 0*/
#endif

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */
uint16_t dac_value;
uint16_t adc_value;
char lamik_dane[17];
int16_t temp_int;

//CAN
uint8_t RxData[8];
uint8_t TxData[8];
int datacheck = 0;

enum {tsStop,tsWaiting,tsGetRegisterAddress,tsGetData,tsSendData};
uint8_t DisplayLCD[18];
uint8_t currsorX = 0;
uint8_t currsorY = 0;
uint8_t transferState = tsStop;
uint8_t registerAddress = 0;
uint8_t transmitBuffer = 0;
uint8_t receiveBuffer = 0;
uint8_t DataLength = 0;
uint8_t Data[6];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
void MX_FREERTOS_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

FDCAN_RxHeaderTypeDef RxHeader;
FDCAN_TxHeaderTypeDef TxHeader;

void LED_Init(void)
{
	HAL_GPIO_WritePin(GPIOJ, GPIO_PIN_10, GPIO_PIN_RESET);
	GPIO_InitTypeDef GPIO_InitStruct = {0};
	GPIO_InitStruct.Pin = GPIO_PIN_10;
	GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
	HAL_GPIO_Init(GPIOJ, &GPIO_InitStruct);
}

void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
 HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData);
 if (RxHeader.DataLength == 8)
 {
 	datacheck = 1;
 	strcpy(DisplayLCD,"Recived");
 	SendToLamik(DisplayLCD);
 }

}

int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */
/* USER CODE BEGIN Boot_Mode_Sequence_0 */

/* USER CODE END Boot_Mode_Sequence_0 */
/* Enable the CPU Cache */

 /* Enable I-Cache---------------------------------------------------------*/
 SCB_EnableICache();

 /* Enable D-Cache---------------------------------------------------------*/
 SCB_EnableDCache();

/* USER CODE BEGIN Boot_Mode_Sequence_1 */

/* USER CODE END Boot_Mode_Sequence_1 */
 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

/* Configure the peripherals common clocks */
 PeriphCommonClock_Config();
/* USER CODE BEGIN Boot_Mode_Sequence_2 */
/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of
HSEM notification */
/*HW semaphore Clock enable*/
__HAL_RCC_HSEM_CLK_ENABLE();
/*Take HSEM */
HAL_HSEM_FastTake(HSEM_ID_0);
/*Release HSEM in order to notify the CPU2(CM4)*/
HAL_HSEM_Release(HSEM_ID_0,0);
/* wait until CPU2 wakes up from stop mode */

/* USER CODE END Boot_Mode_Sequence_2 */

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_MDMA_Init();
 MX_I2C1_Init();
 MX_LTDC_Init();
 MX_USART1_UART_Init();
 MX_I2C4_Init();
 MX_DAC1_Init();
 MX_DMA2D_Init();
 MX_FDCAN1_Init();
 //MX_FDCAN2_Init();
 MX_SPI1_Init();
 MX_TIM3_Init();
 MX_TIM5_Init();
 MX_TIM6_Init();
 MX_UART4_Init();
 MX_UART8_Init();
 MX_CRC_Init();
 //MX_I2C2_Init();
 MX_SPI2_Init();
 MX_TIM15_Init(); //Podświetlanie PULSE 0-998 MAX TIM15.CCR1 = Your_new_pulse_value;
 MX_FATFS_Init();
 MX_RNG_Init();
 MX_FMC_Init();
 MX_JPEG_Init();
 MX_RTC_Init();
 MX_ADC1_Init();
 MX_ADC3_Init();
 MX_TouchGFX_Init();
 /* Call PreOsInit function */
 MX_TouchGFX_PreOSInit();
 /* USER CODE BEGIN 2 */

 if (BSP_SDRAM_SingleTest() != 0)
 {
	 // Error_Handler();
 }

 if (CSP_QUADSPI_Init() == HAL_OK) {
	 CSP_QSPI_EnableMemoryMappedMode();
 }

 if (HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1) != HAL_OK)
 {
 /* PWM Generation Error */
 Error_Handler();
 }

 LED_Init();

 if (HAL_TIM_Base_Start_IT(&htim3) != HAL_OK)
 {
 /* Starting Error */
 Error_Handler();
 }

 if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
 {
 Error_Handler();
 }

 TxHeader.Identifier = 0x10;
 TxHeader.IdType = FDCAN_STANDARD_ID;
 TxHeader.TxFrameType = FDCAN_DATA_FRAME;
 TxHeader.DataLength = FDCAN_DLC_BYTES_8;
 TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
 TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
 TxHeader.FDFormat = FDCAN_FD_CAN;//FDCAN_CLASSIC_CAN;
 TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
 TxHeader.MessageMarker = 0;

 HAL_DAC_Start(&hdac1, DAC1_CHANNEL_1);

 HAL_ADC_Start(&hadc1);
 HAL_ADC_PollForConversion(&hadc1, 20);

 HAL_I2C_EnableListen_IT(&hi2c4);

 /* USER CODE END 2 */

 /* Init scheduler */
 osKernelInitialize();

 /* Call init function for freertos objects (in freertos.c) */
 MX_FREERTOS_Init();

 LamikTask_Init();
 LamikQueue_Init();
 LEDTask_Init();
 LEDQueue_Init();
 EGTLTask_Init();
 EGTLQueue_Init();
 EGTRTask_Init();
 EGTRQueue_Init();

 /* Start scheduler */
 osKernelStart();

 /* We should never get here as control is now taken by the scheduler */
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}


void FreeRTOSLoop()
{
	temp_int = Max31855_Read_Temp(TempL_GPIO_Port,TempL_Pin) ;
	SendToEGTL(temp_int,ErrorMax31855);
	temp_int = Max31855_Read_Temp(TempR_GPIO_Port,TempR_Pin) ;
	SendToEGTR(temp_int,ErrorMax31855);


 TxData[0] = 0x10;
	 TxData[1] = 0x20;
	 TxData[2] = 0x30;
	 TxData[3] = 0x40;
	 TxData[4] = 0x50;
	 TxData[5] = 0x60;
	 TxData[6] = 0x70;
	 TxData[7] = 0x80;
	 if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData) != HAL_OK)
	 {
	 	Error_Handler();
	 }
	 strcpy(DisplayLCD,"send");
	 SendToLamik(DisplayLCD);
	 osDelay(500);
	 
 strcpy(DisplayLCD,"stop");
	 SendToLamik(DisplayLCD);
 	osDelay(500);
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 __HAL_RCC_SYSCFG_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
 |RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;
 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 240;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 24;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
 HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_PLL1QCLK, RCC_MCODIV_1);
}

/**
 * @brief Peripherals Common Clock Configuration
 * @retval None
 */
void PeriphCommonClock_Config(void)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC|RCC_PERIPHCLK_LTDC;
 PeriphClkInitStruct.PLL3.PLL3M = 10;
 PeriphClkInitStruct.PLL3.PLL3N = 181;
 PeriphClkInitStruct.PLL3.PLL3P = 2;
 PeriphClkInitStruct.PLL3.PLL3Q = 2;
 PeriphClkInitStruct.PLL3.PLL3R = 4;
 PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_0;
 PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL3VCOWIDE;
 PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
 PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL3;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}

 

 

 

 

 

 

I cant send or recived data. When canfilterconfig.FilterID1 = 0x100; and i send data from secound board riverdi lcd frozen and i can only reset board. But when i change to other ID like 0x101 no frozen.  Callback Can is never performed

 

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

I see in your code this commented line:

 //hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK; //I try too

What was the result? 

How did you connect the Board to the CAN bus? is there another node connected on the bus? if not for sure it will never work as the acknowledgement mechanism needs that the recipients acknowledge the frame.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
July 5, 2024

Hello,

I see in your code this commented line:

 //hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK; //I try too

What was the result? 

How did you connect the Board to the CAN bus? is there another node connected on the bus? if not for sure it will never work as the acknowledgement mechanism needs that the recipients acknowledge the frame.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.