2024-04-22 6:23 AM - last edited on 2024-07-05 1:39 AM by mƎALLEm
Hello everyone,
I'm currently facing a puzzling issue with the Flexible Data-rate Controller Area Network (FDCAN) on the STM32H755ZI board. Despite using the exact same code that works flawlessly on the STM32H753 board, I am unable to get the FDCAN to function properly on the H755ZI.
Symptoms:
Setup Details:
This behavior is quite baffling. The internal functions seem to work, but there's no physical output on the CAN bus lines. Has anyone else encountered a similar issue with the H755ZI or has insights into potential causes? Could there be a specific configuration or hardware issue unique to the H755ZI affecting FDCAN functionality?
I would greatly appreciate any insights, suggestions, or shared experiences that might help resolve this issue.
Thank you in advance for your assistance!
2024-07-05 1:16 AM
Hello @macsdeve .and sorry for the late answer.
There is no issues with FDCAN on H755 except the ones mentioned in the errata.
Setup Details:
- Board Used: STM32H755ZI
- Environment: Standard setup with external transceivers connected to CAN_H and CAN_L.
Well, you need to give more details about your HW. Schematics is recommended to help you efficiently.