STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EXTERNAL OSCILLATOR

 I AM USING STM32F407G-DISC1 BOARD FOR DEVELOPING CUSTOM BOARD.HERE AN OSCILLATOR IS CONNECTED TO PH1 AND PH2 PINS. IS IT IS COMPALSORY FOR DEVELOPING CUSTOM BOARD?

Resolved! No activity observed in Tx pin of FDCAN in STM32G491KCU6

Hi STM Expert, We are currently working on STM32G491KCU6 MCU FDCAN side. Our requirement is to validate the activity on Tx and Rx pins. We started off the testing with the LoopBack mechanism but unfortunately we were not able to see any data received...

ssuresh by Associate II
  • 14852 Views
  • 28 replies
  • 1 kudos

Resolved! Power cycle required to enter DFU

I am working on a board containing two STM32F412, and I am having a hard time reaching the DFU bootloader:If I power off the board, pull the boot pin low, and then power on the board directly via USB, then cubeProgrammer is able to connect to the boo...

mjuels_0-1729539811093.png mjuels_1-1729540189722.png
mjuels by Associate III
  • 3345 Views
  • 5 replies
  • 2 kudos

Resolved! How can i get a STM32F722xx reference schematic?

I'm trying to use the 64pin STM32F722 part for the first time this time.I need EVM schematic and User's manual for reference circuit.But I can't find the document.Please tell me how I can get the documents.(I could find the reference schematic for th...

KimSuB by Associate
  • 1292 Views
  • 2 replies
  • 0 kudos

Resolved! Project does not start at specified address

Hello.I am using STM32C031.I have set up two projects to be one .bin file based on the attached document.This time I want to output a .bin file for the boot program (addresses: 0x08000000~0x08003FFF) and the application program (addresses: 0x08004000...

shank by Associate III
  • 3038 Views
  • 4 replies
  • 1 kudos

Required Certification?

STM32F038F6P6 - Does the mentioned microcontroller have any certifications, particularly UL certification, which is not explicitly listed on its datasheet or its website?If there are any, please mention.

Resolved! B-G431B-ESC1 Max voltage

Is it possible to input 7S into a B-G431B-ESC1 EVM with a voltage specification that says up to 6S?If not, if I replace some parts with a high rated voltage as below, can I input 7S into EVM? 1. Power Section, TVS diode, SMM4F26A (D20) -> SMM4F33A 2....

Choibogue_0-1730081157127.png Choibogue_1-1730081157128.png
Choibogue by Associate II
  • 8592 Views
  • 12 replies
  • 0 kudos