STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! OCTOSPI interface for communication with a FPGA

Hi AllI have created a PCB where I want to use the OCTOSPI to communicate with a FPGA.I have difficulty finding accurate information on how the different memory types work. I already have a Hyperram running so I started there, that did also seem stra...

Kvang_2-1723555880449.png Kvang_1-1723555699939.png Kvang_0-1723555242998.png
Kvang by Associate III
  • 5200 Views
  • 8 replies
  • 3 kudos

IWDG findings

[This is a reconstruction of a thread I've started on Mar 26, 2017, but got lost in the two forum software transitions since then.]Reports in IWDG short period (125 us) problem  and STM32F407 : IWDG and erase flash sector  indicate that the IWDG does...

HAL_CAN_Start(&hcan) returns error 0x01

Dear all,   I'm using stm32f412ret6 MCU in my custom made board. The code used is as below. The HAL_CAN_Start function returns HAL_ERROR. when debugged the issue is timeout with in the HAL_CAN_Start function. I don't understand if I'm going wrong any...

Aarra.1 by Senior
  • 8384 Views
  • 10 replies
  • 1 kudos

Category device type for FLASH

I am using an STM32G473MEY3 MCU. I am looking in the reference manual in the FLASH section, but I am not sure if this is a cateogry 2, cateogry 3, or category 4 device. I am thinking category 3. Any ideas?

tomm5771 by Associate III
  • 1814 Views
  • 2 replies
  • 1 kudos

STM32 G0B1KEU6: Using LSI as clock source

I am trying to use the LSI as the clock source on the STM32 G0B1KEU6. It doesn't work, and as soon as I select the LSI in the MUX on the clock tree, my code stops working. To ensure there are no other sources of error, I used the exact same code but ...

KarineBlier_0-1729627117840.png KarineBlier_1-1729627125157.png 1.png 2.png

Resolved! Looking for Compact, Low-Power Alternative to STM32F401CCU6

Hello everyone,I'm currently using the STM32F401CCU6 in my project, but it's proving to be oversized for my application, both in terms of physical package and power requirements. I'm hoping to switch to a smaller STM32 microcontroller that maintains ...

ward by Associate II
  • 2513 Views
  • 4 replies
  • 0 kudos

STM32F373 SDADC Output is always 32767

Hi all,I am trying to activate SDADC on my custom designed board to measure a couple of analog voltages. I am trying to measure 5-channels in injected continuous mode. Offset = 0, Gain = 1, Single-Ended Offset Mode. See the CUBE settings below :In th...

MehmetErol_0-1730370624595.png MehmetErol_1-1730371154301.png