STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Chinese fake chip!

China has many chip likes stm32:GD32 AMP32 etc. The bad people use laser to change the Chinese chip into STM32it is vrey bad. I also bought the fake one.

RaidenMEI by Associate II
  • 2013 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H74x/75x SDRAM (re-)mapping and caching

Hello,maybe this MCU is pretty old but... I'm designing HW for the H75x using SDRAM on bank 1 (SDCKE0+SDNE0).RM0433 table 154 shows text "SDRAM bank 1" at 0x7000.0000 and 0xC000.0000, also figure 98 but table 7 "Reserved or remap of SDRAM Bank 2".Q1:...

RM0433_table154.png RM0433_figure98.png RM0433_table7.png
regjoe by Senior II
  • 5375 Views
  • 10 replies
  • 0 kudos

New ST website is horrible.

"Modern feel and look" prevailed over usability, navigability, and common sense. The fact, that the site nags about obsolete browser is a clear indication of the level of incompetence of the creators.Should anybody from ST answer, please do so under ...

Resolved! B-U585I-IOT02A USB Host problem

I'm using BSP driver for USB PD (TCPP03-M20) on the B-U585I-IOT02A, for initialization of the USB PD as USB Host I use the following code:BSP_USBPD_PWR_Init (USBPD_PWR_TYPE_C_PORT_1); BSP_USBPD_PWR_SetRole (USBPD_PWR_TYPE_C_PORT_1, POWER_ROLE_SOURCE)...

milorad by Associate III
  • 2913 Views
  • 6 replies
  • 3 kudos

Resolved! MCU stall after a number of continuous writes to FMC

Hello all, I faced with a big stall issue when write a number of data via FMC. I guess it is related somehow with a cashe controller, but I can be wrong.The details in brief:I use an STM32H757 std dev board with all needed corrections to apply FMC in...

LeonidP by Associate III
  • 1349 Views
  • 1 replies
  • 0 kudos