hianyone help me how to use 2 channel of input capture of timer 3.i am giving two different external digital pulses to input capture of channel 1 and channel 2.as currently if i use independently these two channel one by one, they are working ok. if ...
hiwe have requirement of SIL2/ SIL3 verified microcontroller which have 24 adc channel, UART(2), ETHERNET, CAN(2),SPI,I2C, 512KB FLASH ETC.kindly suggest us
hicould you please brief what Input filter will do with input capture data? how input capture data will affect using this filter and without using this filter?
hifollowing is my code. both capture input has different frequency from two different hall type speed sensor output.when i use either only one it works fine but when i take capture input from both then my frequency output is varied. like(exact outpu...