STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! H723..H735: functions in ITCM, strange behaviour

Heyho,I recently found that I'm not using ITCM RAM at all, then started to put heap and stack there.No problems so far.Then I copied some functions there, and all went well - until I found some strange behaviour:1..4 SAI RX DMA transfers running, cir...

LCE by Principal II
  • 373 Views
  • 5 replies
  • 2 kudos

STM Virtual Com port win11 driver needed

hello, where can i download win11 STM virtual com port?  i install both VCP_V1.5.0_Setup_w7_x64_64bits and W8_x86_32bit all not working ! i din seeSTM Virtual Com port at device manager! only STM STLink visual com port appear ... 

StanJerm by Associate III
  • 53609 Views
  • 12 replies
  • 3 kudos

Resolved! Internal Temp Sensor STM32H563VI

Dear ST Community,I am currently migrating my Firmware from STM32H723VG to STM32H563VI. I have problem with Internal Temp Sensor. Based on Reference Manual on both MCU reading temperature is the same, but it doesn't work as it should.When on STM32H7 ...

adakPal by Associate III
  • 453 Views
  • 6 replies
  • 2 kudos

Resolved! Timer cascading not working as expected

I'm working on a design with an STM32L072CZT6TR, where I want to calibrate my main timebase. That main timebase is TIM6, which counts 16,000. The HSE is 16MHz, so there's an interrupt evey 1ms. Calibration is done by counting the number of HSE cycles...

RobK1 by Senior II
  • 252 Views
  • 2 replies
  • 1 kudos

Resolved! CAN BUS on Nucleo H743ZI2 - clock configuration issue

Hello,I’ve recently started using ST products and the IDE with CubeMX, which is why I’m asking for your help. I’ve just begun developing a communication system using a Nucleo H743ZI2; my goal is to set up a UART and a CAN bus.The UART is done; I used...

Forum_ST_1.png Forum_ST_2.png
AmGo by Associate III
  • 763 Views
  • 12 replies
  • 8 kudos