STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IAP over SPI stm32u5

 I need support to get IAP over SPI.I've esp connected to my stm32u5 over SPI. Stm is slave and ESP is master. For stm I've created project using stmcube by entering MCU part number.Now here my question is1. Do I need to develop bootloader code to ac...

Resolved! CE Certification STM32G071RB

Hello,I am currently preparing the documentation package for CE certification of a device that uses the STM32G071RB microcontroller.Could you please clarify whether there is any official CE compliance documentation available for this MCU (or for the ...

yz_89 by Associate
  • 196 Views
  • 1 replies
  • 1 kudos

Resolved! STM32G411 availability?

I see in STM32CubeMX that a STM32G411 exists but it has the status "restricted". I'm curious why this type is not widely available. I'm currently using the STM32G431 in an application, mainly because of its raw clock speed of 170MHz. I don't actually...

MarcV by Associate II
  • 441 Views
  • 3 replies
  • 7 kudos

Resolved! STM32U5G9ZJT6Q Footprint Confirmation

Hi Team,I'm recently using the STM32U5G9ZJT6Q part in one of my design. I couldn't find the package mechanical information in Datasheet. For now, I'm using the LQFP-144 form the STM32H573ZIT3Q part number. Will it be okay? Can you please help to veri...

Resolved! GPIO output speed

New programmer and new to the STM32 ecosystem as well.I am working with a STM32F401 as it has 5v tolerant inputs and 2 32bit clocks.I have a simple program that reads the 2 32bit TIMs (2&5) in encoder mode, sums the results and then outputs a quadrat...

LANLocked by Associate II
  • 861 Views
  • 13 replies
  • 7 kudos