STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Write into flash while USART interrupt executed

Posted on October 23, 2017 at 12:33 Hello, I have some trouble to write into the flash of my stm32f I can send via usart a lot of commands to the µC, interprete and execute them finally. One command is to write some data into the flash but if I w...

Resolved! Differences between hardware interrupt and hardware event

Posted on October 26, 2017 at 18:49Hello,I am using an STM32F4 MCU and I have a doubt regarding the hardware event .The datasheet http://www.st.com/content/ccc/resource/technical/document/reference_manual/3d/6d/5a/66/b4/99/40/d4/DM00031020.pdf/files...

simo zz by Senior II
  • 1415 Views
  • 1 replies
  • 0 kudos

CubeMX Feature Request: Add CAN TTrig Functionality

Posted on October 26, 2017 at 18:54I would be nice to have access to the timing features present when using Time-Triggered Mode on the CAN modules. Specifically the RDTR and TDTR registers. Additionally, why not simply make copies of the registers a...

How to receive data from master SPI

Posted on October 26, 2017 at 18:17I'm trying to configure my STM32L4 as an SPI slave and am having some difficulty. I've integrated the SPI_FullDuplex_ComDMA sample into my application and configured my device as a slave. I can also use my Aardvark...

Konami by Senior II
  • 767 Views
  • 0 replies
  • 0 kudos

STM32F103 WR SPI EEPROM

Posted on October 26, 2017 at 15:59Hi, I try to use STM32F103 SPI interface to write and read SPI EEPROM, I don't know where can get the example source code for it?Best Regards,Kent#spi-write-and-read

kent gu by Associate III
  • 792 Views
  • 1 replies
  • 0 kudos

STM32CubeL4

Posted on October 25, 2017 at 03:11STM32CubeL4 1.10 is listed on the website, but version 1.9.0 is inside the .zip file when downloaded.

ax0018 by Associate III
  • 4366 Views
  • 11 replies
  • 0 kudos

STM32F334 HAL DMA ADC Scan conversion not working

Posted on October 09, 2017 at 20:26Hello. In my project, I use the ADC configured in scan mode, as seen on this screenshot from STM32CubeMX:and the DMA configured as follows:The problem is that I can't get any data transferred from ADC to memory, wh...

0690X00000608XgQAI.png 0690X00000608XRQAY.png
RichardS1 by Associate II
  • 2109 Views
  • 3 replies
  • 0 kudos