hi everyone i'm using STM32L4A6RG controller ,in this MCU have USB OTG support ,in my project im using USB device only ,code also cubeMX code only ,while using USB device ,serial port it's connected but after some times MCU automaticall...
Hi i'm using STM32L452RE controller ,i'm try to connect(through VCP ) USB (device ) with our own windows application that time it showing error like USB driver it not 32 bit , but i'm installed virtual com port driver ver 1.5.1 only . i need .inf 3...
Posted on November 09, 2017 at 11:30Hello All,While build my project i got some error like below,but in application level no error . I am using the below environment1) NUCLEO L476RG2) IDE: System Workbench on STM32 3) updated AC6 plugins Error Messa...
Posted on August 24, 2017 at 09:06Hi, i am using STM32L476VG DISCOVERY board ,i am try to connect VCP(virtual com port ) user USB to PC(win XP & win 7) i also installed virtual com port driver from STM website (en.stsw-stm32102) but my board(user U...
hi ,Thanks for your reply ,im my previous project they using Modem driver(it's microprocessor and that linux base ) Now i'm working in Micro controller ,i should use previous windows softer ware only