User Activity

The murata Lora module CMWX1ZZABZ is used and the STM32L072 is inside.Can the STM32 internally reset itself without using the reset function?Explain what happens if a reset occurs.
Posted on April 09, 2018 at 04:17Hi.I am going to set the RDP-Level 1 programmatically.Here is the test code:Here it stops at the HAL_FLASH_OB_Launch () function.The Reset button does not work in this state.The USB connection will work only if you r...
Posted on April 05, 2018 at 03:50Hi.I am going to set the RDP-Level 1 programmatically.Here is the test code:Here it stops at the HAL_FLASH_OB_Launch () function.The Reset button does not work in this state.The USB connection will work only if you r...
Posted on January 31, 2018 at 09:04HI.I am testing with ST Discovery LoRa Kit, PingPong.There is no problem sending / receiving 64 bytes.However, the size of 64 bytes or more can not be transmitted or received.Semtech says that 128 bytes are possibl...
Posted on December 13, 2017 at 08:23I have a nucleo-L073RZ board.Boot0 port, Flash loader is being used to download the firmware.Connecting with USART1 (PA9, PA10) works well.However, it can not be connected to USART2 (PA2, PA3).In the AN2606 docume...