STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Boot from SRAM

Posted on October 23, 2017 at 10:49I have a question about the stm32f103xx. I want to know how it boots from Embeded SRAM. I have known that the IBUS of Cortex-M3 can't access the SRAM from the reference manual. When boots from the SRAM,  how Cortex...

l yk by Associate II
  • 6244 Views
  • 14 replies
  • 0 kudos

Disable STM32F103 Independant Watchdog

Posted on October 19, 2015 at 11:01Hello,In one of our projects we have implemented IWDG (independant watchdog). There is a condition in the software that when the power supply fails, the controller STM32F103(Powered By Rechargeable Battery) puts it...

gada by Associate III
  • 4002 Views
  • 4 replies
  • 0 kudos

nucleo board communicate with raspberry pi through SPI

Posted on October 27, 2017 at 14:57the task is to make nucleo board L476 to commucate with raspberry pi 3 through SPI. Now the code on both sides are finished and build successful. But I don't know how to test if the data are sent successfully. Is t...

Shared memory between BL and Main application

Posted on October 19, 2017 at 10:46 I am working on the project with STM32F030R8T6. So far I have bootloader and main application with memory space allocated. My problem is that currently I am jumping between main and bootleader using address of re...

Resolved! CubeMX USB_DEVICE middleware problem on V1.9.0

Posted on October 27, 2017 at 13:25Hi, I just moved a code from a STM32L476RCT6 on cubeMX V1.7.0 to V1.9.0I didn't change anythingWhen I start the push and start the program, it crash on the SystemClock_Config() with the new version. I tried again w...

Move source code and issue tracker to github

Posted on October 23, 2017 at 11:56I suggest to move relevant/related projects (STM32CubeMX, HAL, LL libraries, etc?) to github.Reasons:1. It is (arguably) one of the best places to host opensource projects.2. It has great issue tracker3. Thus, it i...

Store RTC date into Backup Register

Posted on October 25, 2017 at 12:09 Hi there, I'm using the RTC on my STM32F103 to keep the date and time but when I reset the MCU the date is lost. I know that this behaviour is due to the RTC implementation ( it uses a counter ). To prevent...

Fede Rico by Associate III
  • 4348 Views
  • 15 replies
  • 1 kudos

stm32f7 and SDRam

Posted on November 23, 2015 at 18:38The original post was too long to process during our migration. Please click on the attachment to read the original post.

Resolved! USB Report Length

Posted on October 25, 2017 at 21:34I have the USB HID demo working on an STM32F072B-DISCO board. I grabbed the code from the HID demo app to make a custom Windows project. Everything works alright, but I want to increase the report length (the demo ...