STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Sending float32 with UART

Posted on January 03, 2017 at 18:47Hi there, recently I was making acustic spectrometer using STM32F4-Discover. In my project im making FFT with 'arm_math' libraries and then I need to send data to PC (with which I'll display it) via UART.After maki...

Tom G by Associate
  • 5668 Views
  • 7 replies
  • 0 kudos

STM32F373 Timer questions

Posted on June 24, 2014 at 16:58Hello,I have a timer performing input capture on one channel. Can I set another channel OF THE SAME TIMER as an output with a frequency double of the captured input signal frequency?-------------I am not 100% clear on...

ing by Associate II
  • 2358 Views
  • 5 replies
  • 0 kudos

CAN -> How to send overload frame?

Posted on August 15, 2017 at 05:00Hi,has anyone ever managed to send a standard CAN overload frame on an stm32?So far, I could only find error handling for incoming frames but no way to send one myself.#can #overload

Can not connect to device

Posted on October 24, 2017 at 08:53Hi, I use ST-Link V2 eumlator and STM32 ST-Link Utility SW to flash STM32F103VE. At the beginning, it can flash for several days. Today it can connect to device(show device information), but can't flash. It show ca...

0690X000006049pQAA.jpg
kent gu by Associate III
  • 1745 Views
  • 4 replies
  • 0 kudos

Resolved! PWM shift or move question

Posted on October 25, 2017 at 13:08Dear all,I am programing a STM32F429 for creating 4 PWM for inverter aplication. I managed to create these 4 PWM using TIMER1 and channel 1, channel 2, channel 1 N and channel 2 N.The inverter works pretty good usi...

STM32F103 internal bootloader work on RS485?

Posted on October 25, 2017 at 16:32Hi,I am using STM32F103RET6 microcontroller. On my PCB, the USART1 channel is used as RS485 communication with a SN65HVD11HD transceiver.  That means to transmit/receive each character, the direction pins RE, DE pi...

Jian Chen by Associate II
  • 1272 Views
  • 1 replies
  • 0 kudos