STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART Reception bytes missing

I am trying to receive variable length of data by manipulating the the RxXferCount value and pRxBUffPtr.I am getting desired results most of the time but for certain time the receive buffer is unable to capture all the bytes i sent.I tried to debug i...

SYLVIA by Associate II
  • 1090 Views
  • 1 replies
  • 0 kudos

Trouble establishing I2C communication between 2 STMs

I am trying to establish I2C communication between 2 STMs. The master is NUCLEO-L432KC and the slave is NUCLEO-L412KB. I changed the address of slave in cubeMX to 0x01 which is in the 7-bit address format. But I am not able to send or receive data. ...

Need reference project for STM32F746-Discovery

I can't get the sample running on my stm32F746-discovery. I followed the instructions in https://www.youtube.com/watch?v=43qQhrXc3n4.After changing MX_QUADSPI_Init(void) to the values inthe stm32746g_discovery_qspi.c I get a picture with a button but...

0690X00000AqpyaQAB.jpg
Andi by Associate III
  • 1218 Views
  • 1 replies
  • 0 kudos

Resolved! Internal flash failing after 60 - 70 erase/write cycles

Hi,I am currently facing an issue on a STM32F469NI MCU where the HAL_FLASH_PROGRAM() is succeeding yet fails to write to the flash memory.I have verified this with a basic project for the STM32F469Discovery to isolate hardware. It appears that after ...

JHedges by Associate III
  • 2880 Views
  • 5 replies
  • 0 kudos

STM32L4R9I-EVAL Problems to use UART1 PB7 (rx) and PG9 (tx)

Dear community,I've been playing with the STM32L4R9I-Eval board and it seems that I can't drive the PG9 pin.My plan is to use the UART1 with the following pins:PB7 (rx) PG9 (tx).I checked the documentation and to use PG9 you have to:Remove R236Open S...

0690X00000ArdKLQAZ.png
LPers by Associate II
  • 2389 Views
  • 5 replies
  • 0 kudos

TIM1 ch1 as pwm, ch2 as cc to trigger adc caputre

On STM32F105 chip, i need to output a pwm, then adc caputure the voltage on pwm high stable level.So i try to set tim1 ch1 to pwm out, and then set tim1 ch2 as compare output wih no pwm to trigger adc capture with DMA. (CC2<CC1)Eventrually, i cannot ...