STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750B-DK not able to program using system workbench

I have purchased STM32H750B-DK. I am using system workbench for stm32 as IDE. Now i downloaded STM32CubeH7 library and trying to download GPIO_IO_Toggle example program into this board but getting the error as below:17:31:42 **** Programming project ...

VAgga by Associate II
  • 2682 Views
  • 5 replies
  • 0 kudos

Circular DMA seems to "doublebuffer" (STM32F427)

What is it that I've been missing...I set a timer to trig 7-channel ADC with DMA. The DMA is set to make 7 16-bit to 16-bit transfers circularly. It seemed to work fine, but some data started to corrupt. So I made the 7x16-bit buffer 4-fold (28 16-bi...

SDMMC 4 bit mode with DMA (STM32L4R7)

Hi,I'm trying to configure SDMMC module using DMA since I'm using FREERTOS. But in STM32CUBEMX, there is no option to configure DMA settings under FATfs.So, I'm trying to setup the DMA configuration through code. I can see that there is no definition...

Iswarya by Associate II
  • 1682 Views
  • 1 replies
  • 0 kudos

STM32CubeL4 SubGHz P2P missing data

Hi,I have two B-L475E-IOT01A boards and I am testing the SubGHz P2P application available in the STM32CubeL4 package. Whenever I press the User Button on one board the led LD1 on the other board blinks, and as the ACK command is received the led LD1 ...

VREFINT_DATA

I'm using the STM32F0 Discovery (STM32F051R8T6) and trying to measure temperature via an ADC input. We're using the formula: VChannel = (3.3V * VREFINT_CAL * ADC_DATA) / (VREFINT_DATA * fullscale), but we are unsure what to use as the VREFINT_DATA va...

KLeon.875 by Associate II
  • 2538 Views
  • 5 replies
  • 0 kudos

Configure DMA for MDMA H7 dual core

Sorry to be asking so many questions, but these dual core h7s are hella complicated and the documentation can be a little vague.I am trying to understand how to set up the dmas to work with the mdma. I think i get the dmamux and how the mdma works wi...

RMcCa by Senior II
  • 896 Views
  • 0 replies
  • 0 kudos

STM32F769 no MCLK out from SAI

Using the STM32F769I-DISC1 evaluation board I am trying to use SAI1 to output a TDM audio stream. I know the CODEC doesn't support that format but my production board will need it.When configured as master transmitter, I get good SCLK, data and fram...

Alan3 by Associate
  • 1276 Views
  • 2 replies
  • 0 kudos