STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 HAL_EXTI_SetConfigLine() causes the Hard Fault

STM32F7 HAL_EXTI_SetConfigLine() causes a Hard Fault whenever the parameter is one from the HAL_EXTI_GetConfigLine(). CubeIDE 1.2.1STM32Cube FW_F7 V1.15.0Nucleo F746Following is the sample of the sequence. This code retrieve the EXTI configuration of...

Takemasa by Associate III
  • 1276 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F3xx - Hardfault_Handler due to failed vector table fetch

First I want to say that I am a newbie in this field. I am trying to upload and debug a code on a custom-made board based on STM32F303CB chip through a NUCLEO-F446RE board. I am using Eclipse IDE (2019-12), a GNU toolchain and a SEGGER J-Link debuggi...

SVasi.1 by Associate II
  • 5932 Views
  • 6 replies
  • 0 kudos

Resolved! How to configure PWM as Gated output?

Hi,I am using STM32F072VBT6. I need a PWM waveform output that is gated with a PWM output of another timer channel.I am using TIM3_CH1 as the master that will control the output of another PWM of TIM2_CH1. Please refer the image for clarity. I need w...

0690X00000DXUt4QAH.jpg

the RM0090 reference manual for 2014 ,in the description of the “Chip Select togglest�? different from RM00990 reference manual for 2018,why?

the RM0090 reference manual for 2014 ,in the description of the “Chip Select togglest�? different from RM00990 reference manual for 2018,which one is correct?The results of our tests are consistent with reference manual for 2014,Is it wrong in RM0099...

0690X0000087VffQAE.bmp 0690X0000087VfaQAE.bmp
cxiao.6 by Associate II
  • 3864 Views
  • 8 replies
  • 0 kudos

I have a question,when changed cpu from stmf407 to stm32f427 .sometimes, read a wrong data from extern sram access by FMC ,it's happend in most of the cases in interrupt ,someone have the same problem?

my English is poor,In the same program ,cpu 407 do not have this problem,only happened in 427​,somtimes.It's like 2.3.4 Corruption of data read from the FMC. in <Errata sheet - STM32F42xx and STM32F43xx - STM32F427/437 and STM32F429/439 line limitati...

cxiao.6 by Associate II
  • 2374 Views
  • 4 replies
  • 0 kudos

printf function call causes hard fault

Hi all,I am working on a STM32F103VEtx MCU. In my firmware I have redirected the printf function to a UART for debugging purposes. When I start running the code, the printf function causes the hard fault handler to hit. Please see the call stack att...

0690X00000DXN5RQAX.png

Effect of timer CCR not in range 0<CCR<ARR

DMA requests are still generated if the CCR is outside the auto-reload rangeThe DMA request is is generated when CNT reaches 0 rather than being disabled.Processor is a STM32H750is this a bug or a feature - it should be documented anyway

pbayton9 by Associate III
  • 1587 Views
  • 2 replies
  • 0 kudos