STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Effect of timer CCR not in range 0<CCR<ARR

DMA requests are still generated if the CCR is outside the auto-reload rangeThe DMA request is is generated when CNT reaches 0 rather than being disabled.Processor is a STM32H750is this a bug or a feature - it should be documented anyway

pbayton9 by Associate III
  • 1604 Views
  • 2 replies
  • 0 kudos

Trying to go into, then out of sleep mode. Two problems.

Problem 1)  current draw does not change after entering sleep mode.Problem 2)  not sure if program should resume where it stopped or from the beginning of main. Also any difference between waking by NRST or by A0 set to PWR_WKUP0?Mcu is 'H747 operati...

PAngl.14 by Associate II
  • 1357 Views
  • 2 replies
  • 0 kudos

Please order with newest first as default!

Hello,https://www.st.com/en/microcontrollers-microprocessors.html#resourcestarts with some unknow order. Clicking on the "Latest update" results in the oldest on top. Only with a second click, the newest entries git first. These resources are mostly ...

[TIM] how to read current TIxF state

I want to know the current level of the channel-input filter's output, marked as TIxF on the diagrams and in narrative.I know I could read the respective pin, but that's not the same - it misses the filtering aspect, i.e. a single read might inadvert...

STM32L475 Multiple wake up interrupts for stop2 mode.

Hi Community,I am working on deveoping applications on STM32 IoT Doscovery kit. I am interested in the lowe power design aspects as far as the sensor reading is concerned. This is my first time working with sleep modes / reducing power consumption. C...

How to know the MCU address for its use as an I2C slave ?

Hi guys, I would like to connect two different MCU to each other through I2C. One MCU would be the master, and the other one the slave. How can I find the I2C addresses of these devices ?I found the device ID in the reference manuals : 0x411 for STM3...

HHUET.1 by Associate II
  • 1444 Views
  • 1 replies
  • 0 kudos

Resolved! Load capacitance (AN2867)

I am working in small startup in Bangalore. I had designed the board using the STM32F103R8T6 controller now i am facing oscillator issue, oscillator is not working as i expected. thereafter i googled it for oscillator design guide and i found AN2867....

Bhat by Associate II
  • 11551 Views
  • 6 replies
  • 0 kudos