STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is the temperature sensor factory calibrated?

We are currently using an F4 (STM32F407IGH6) and an F3 (STM32F303VC) in our product. We want to pull the temperature sensors to get an idea of chip temp. Looking at the datasheets, the F3 data sheet explicitly states that factory calibraiton is done...

0693W000001sZdkQAE.png 0693W000001sZerQAE.png
PCicc.1 by Associate
  • 1024 Views
  • 1 replies
  • 0 kudos

MCU working issue.

I am using STM32F439ZGT6.I have flashed the code to this controller. After flashing the code when I restart (power off and power on ) the MCU first time, that time unit is working absolute fine but if I power off and power on the unit, that time I am...

GAGGA.1 by Associate II
  • 2211 Views
  • 5 replies
  • 0 kudos

Resolved! Behaviour of STM32H743 general purpose timer

Hello,I'm using TIM2 on STM32H743 (Nucleo, rev Y, Keil 5.31).Just before setting the bit TIM_CR1_EN the setting of the timer is the following:DIER : bit UIE setPSC: expected value (0x4E1F)ARR expected value (0x4E20). it is almost the same as PSC but ...

Gpeti by Senior II
  • 3648 Views
  • 6 replies
  • 1 kudos

Resolved! STM32F030C6 wih external oscillator (HSE)

I am trying to understand how to setup the microcontroller (STM32F030 in this case) to use external oscillator. I am using blinking LED as a test to see if the code is running. To setup the HSE I did following:selected Crystal/Ceramic Resonator in Hi...

BJerk.1 by Associate II
  • 1589 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743 IWDG continuously reset MCU

Strange behavior of STM32H743. It continuously reset every few seconds.I check reset reason with this part of code after system startup:if (__HAL_RCC_GET_FLAG(RCC_FLAG_IWDG1RST)) { _PRINTF("RESET_CAUSE_INDEPENDENT_WATCHDOG_RESET\n"); } else...