Skip to main content
CAiwe.1
Visitor II
February 23, 2020
Question

STM32H743ZI QSPI

  • February 23, 2020
  • 0 replies
  • 448 views

MCU is STM32H743ZI. When QUADSPI working in AutoPolling mode,Setting the ABORT bit in the QUADSPI_CR, Why SR.BUSY bit stall high? BUSY don't goes low forever!But according to referrence manual,"In automatic-polling mode, BUSY goes low only after the last periodic access is complete,due to a match when APMS = 1, or due to an abort." My source code is below:

/**************************************************************

* @brief QUADSPI work at status flag polling mode(automatic-polling mode)

* @param cmd: command to send(FLASH Status polling command)

* @retv @0:match; @1: not match,time out.

*****************************************************************/

uint8_t QSPI_StatusPolling(uint8_t cmd,uint32_t timeout)

{

   __IO uint32_t ccr;

   uint8_t retv;

   QUADSPI->DLR = 1; // read data bytes: 1

   ccr = 2<<QUADSPI_CCR_FMODE_Pos; // FMOD=2: status flag polling mode

   ccr |= 1<<QUADSPI_CCR_IMODE_Pos; // Instruction Mode: single line

   ccr |= 1<<QUADSPI_CCR_DMODE_Pos; // CCR.DMODE: Data Mode: single line

   ccr |= cmd;

   QUADSPI->CCR = ccr; // begin access

   while( ((QUADSPI->SR&QUADSPI_SR_SMF_Msk)==0) && (timeout>0) ) // wait until Status Match or timeout

   {

      timeout--;

    delay_us(1);

   }

   QUADSPI->CR |= QUADSPI_CR_ABORT_Msk; // aborts the on-going command sequence

   while(QUADSPI->SR&QUADSPI_SR_BUSY_Msk) {} // wait when SR.BUSY=1 ,stay here for ever!!!!!!!!!!!!

   ccr = QUADSPI->DR;   // clear FTF

   if(timeout==0) retv=1;

   else retv=0;

   return(retv);

}

This topic has been closed for replies.