STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F469i Source Code for Demo Firmware

Hello all,I recently purchased the STM32F469i Discovery Board, and have loaded the compiled demo binary from the ST website onto the board. It loads properly, but now I want to see how the software works. Is there any source code for the demo firmwar...

TLian.11 by Associate II
  • 1416 Views
  • 2 replies
  • 0 kudos

STM32F767 QUAD SPI with DMA2

I'm using STM32F767 and external flash is interfaced on QUADSPI, I've referred STM32746G-Discovery code for QSPI without DMA and its working fine. I want to implement QSPI using DMA, STM32F767 supports QSPI over DMA on channel 3 and stream 7 so did c...

AShel.1 by Associate III
  • 1320 Views
  • 2 replies
  • 0 kudos

Can't wake from stop mode with low power timer event

Hello everyone,I'm having problems with a STM32L010K8 in stop mode.I'm trying to use the low power timer clocked by the LSI and having it to wake up the device from stop mode once the timer reaches ARR value.I configured the EXTI event line 29 and de...

Kraal by Lead
  • 4019 Views
  • 5 replies
  • 0 kudos

stm32L5 SDMMC interface as memory card

Moin, is it possible to run the stm32L5 Series mcus (or other stm32s) not in SDMMC host mode, but be used like a normal SDcard for storage?I looked over the documentation and only found host mode descriptions. I feel like I missed some details, so gr...

ChrisP by Associate II
  • 2364 Views
  • 4 replies
  • 0 kudos

Problems with Initialisation of LSM6DSM and LSM303AGR during debugging of SENSORTILE (STM32L476JG) with on-Board ST-LINKV2/1 of Nucleo-F401RE

Hello all =)I am pretty much a beginner with STM32 microcontrollers and facing some, at least for me, elusive problems during debugging of the controller.I am working with the SENSORTILE, so the STM32L476JG controller, which is soldered onto the crad...

0693W000001sdD2QAI.jpg
AGans.1 by Associate
  • 886 Views
  • 0 replies
  • 0 kudos

IWDG initialization Error.

In my project there is requirement to initialize the IWDG for two times one with time period 5 second in run-mode and re-configuring it for 32 second before controller enters into sleep mode. as shown in below code. hiwdg.Instance = IWDG; hiwdg.Ini...

Rghar.1 by Associate
  • 1946 Views
  • 2 replies
  • 0 kudos

In STM System WorkBench : Can we use 2 different linker scripts , one for Debug Settings and one for the Release setting . Currently there is no option to exclude one linker script when switching between Release Configuration to Debug configuration

In STM System WorkBench : Can we use 2 different linker scripts , one for Debug Settings and one for the Release setting . Currently there is no option to exclude one linker script when switching between Release Configuration to Debug configuration