STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F410RB Timer External clock mode PROBLEM

Hello everyone, this is my first post here. I am actually working on custom pcb with a STM32F410RB, which is used to count an external signal.To do this I use 2 timers, Timer 9 configured in internal clock and counting a 1 second period and generate ...

KOlli.1 by Associate
  • 900 Views
  • 0 replies
  • 0 kudos

What is relation between Bit-Rate and Nominal & Data parameters setting for FDCAN/CAN interface on STM32 H7xx Family?

I'm working on FDCAN & CAN interface provided on H745XI-DISCO board. I was new to these interface when I started, but now I can say I have good understanding on CAN & FDCAN Bus protocol. Using provided examples with STM32CubeIDE FW for H7 series, I w...

JJ1 by Associate II
  • 2514 Views
  • 1 replies
  • 0 kudos

SPI RX->DMA stops running when debugger is allowed to resume

I'm trying to run SPI2 (Master Receive Only) such that it continuously DMAs data from the slave. The problem is, it only works when I step over the HAL_SPI_Receive_DMA line... at which point I see SCLK, and it will run forever, until I "resume" th...

EZamo.1 by Associate III
  • 2304 Views
  • 5 replies
  • 0 kudos