Thanks for your answer.Where can I find the designer start windows? I'm using system workbench which, for what I undestood, is compatible only with 4.10.0.
I'm using system workbench and, for what I have inderstood, it works only with the version 4.10.0. Do the examples that you are citing work also for 4.10.0?
@Community member is suggesting just to disable/add the features on the desidered pin. I think that your answer is more correct ( disable the chips select) but what do you think of simply disabling the PIN (I think that there should be some interfer...