STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

COM Port Terminal Debug Gone in Windows 10

(After installing the virtual com port, cannot access)(Current visual with the recognized STM32 link Ukeil and other tools recognize)I used to see com ports via the device manager in windows 10. I've installed the Link 009 drivers for stm32 boards an...

0693W000005AG0gQAG.png 0693W000005AG10QAG.png
ABeau.1 by Associate
  • 2080 Views
  • 3 replies
  • 0 kudos

Clocked Data receive with SPI or USART?

Hi Guys,I have an F7 and want to read in a data stream. Transfer is synchronous, constantly on and data rate is about 2kBaud. 1 Frame consist of 64 bits, in which i have to find a pattern for the start. I want to use a DMA with maybe 128 bit transfer...

nico by Associate II
  • 1923 Views
  • 3 replies
  • 0 kudos

SPI in slave mode doesn't work correctly (STM32F100RB)

The SPI does not work correctly in the slave mode when CPOL=0 and CPHA=0 or CPOL=1 and CPHA=1.When transmitting some bytes, the slave SPI distorts the data and terminates the processing of the frame prematurely (during the seventh pulse of the clock ...

Resolved! How to disable the M4 core on the STM32H745?

We have to write firmware for a STM32H745. It was not our decision to use a dual-core version and we are pretty sure that a single M7 core will easily do the trick, so the next iteration of the PCB will contain a single core variant. Now we would lik...

cm0x4d by Associate III
  • 5939 Views
  • 8 replies
  • 0 kudos

Try ST evaluation boards remotely!

Hi all!I'm an embedded developer with 15+ years of experience. And now I am working on a project that seems to be useful for developers like me. But there is a great lack of feedback. I'm asking for help from the professional community.What is it: a ...

Resolved! internal DAC (DAC3) connection to OPAMP1 - no output from OPAMP

Hey,I'm using: STM32G431, NUCLEO-G431RBI would like to connect DAC3 - internally to the OPAMP and take the OPAMP1 output. I have an array I want to transfer to the dac3 via DMA, the timing is controlled by tim2. Then having DAC3 to be the non-inverti...

YLivn.1 by Associate II
  • 5138 Views
  • 6 replies
  • 0 kudos

Resolved! We have shortlisted STM32G431CBT3 controller for our new Automotive project. I would like to ask that Does ST provides the driver stack for this controller for free?

We are selecting a controller for our new Automotive project with CAN - FD connectivity, but we want to know whether ST provides the driver stack for CAN - FD for above microcontrollers for free.

HMaka.2 by Associate II
  • 1241 Views
  • 1 replies
  • 0 kudos

STM32 F767Zi RS485 interrupt code blocks main() loop

I am using STM32 F767zi MC and I want to communicate with RS485 encoder. This is my code which has written in stm32f7xx_it.c. When executing this code, it can be seen that encoder and MC communicating continuously (observed using oscilloscope). But ...

KMale.1 by Associate II
  • 1679 Views
  • 3 replies
  • 0 kudos

STM32H743 SRAM physical specification

HiI am planning to run a RAM test on STM32h743 RAM module. But I noticed that the RAM is divided into 3(SRAM 1,2,3) .Are these three RAMs physically different or the same RAM divided into three modules.Thanks in Advance

RK.1 by Associate II
  • 1576 Views
  • 2 replies
  • 0 kudos