User Activity

Hello,I'm currently designing a prototype and due to the short list of functions I need, I felt it could be a good occasion to try STM30G0 series for evaluating power consumption.I choose a STM32G030F ( TSSOP20) and here is what I've seen in the data...
Hello,I was designing a board with a VL6180 and was surprised that the 0x4F register never uptaded to tell me that a new measurement was finished.So I looked at the 0x4D register to see that it answered me 0x19. Whitch mean I have a VCSEL continuity ...
Hello everybody,I need a power conversion DC-DC 24V to 3.3V. So I went to eDesign suite who recommendend me the following architecture:I reproduced it in my design: I produced the board, and when I apply 24V on the input, I obtain only 0.9/1V on the ...
Hello,I will have to set up an electronic design with 2 VL6180X on the same I2C bus.ST provide an interesting document about changing addresses while using RESET lines of this component.I will probably not be able to use this technique due to the geo...
Hello Everybody,I'm building a device who need to transfer a bunch of datas on a CAN bus at 250bauds.When I get the datas from my buffer to create the messages, it seem that some are mission (I'm sniffing the CAN bus with a can-bus shield from seedst...
Kudos from