STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431 Bootloader

Hello , I'm using STM32G431RB, and I am trying to flash the MCU via UART1 using PA9 and PA10 pins but I can't make it work ..I get an error like "Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port confi...

Stefano1 by Associate II
  • 2766 Views
  • 9 replies
  • 1 kudos

Resolved! CAN baud rate change, device is restarting continuously!

Facing issue with CAN baud rate change!1. The Master and slave devices are communicating at baud rate of 1Mbps.2. If I change the baud rate of Master device to any other baud rate(like, 250kbps, 500kbps,125kbps,50kbps) then master device contiguously...

ramji by Associate II
  • 2859 Views
  • 7 replies
  • 3 kudos

Resolved! What is a half-DMA inside the NPU?

From the reference manue, I can find a term half-DMA, but this term is not well described, and I don't know what this half means, what is the difference bewteen a half-DMA and a normal DMA??? Is it just the size or the available target address is sma...

Einstein_rookie_version_0-1750753692420.png

Resolved! Bootloader and Read-while-write (RWW)

Hello,we are using a STM32F429.The bootloader is located in the first 64kB. The firmware in the remaining sectors.It erases the remaining sectors of the flash and writes the new firmware.Now, 3.6.5 Read-while-write (RWW) of the reference manual state...

h p by Associate III
  • 1194 Views
  • 2 replies
  • 0 kudos