User Activity

Folks,Is there a way to have a variable that is incremented each time the project is compiled? I can do this with Rowley Crossworks and it's really useful. I define and major and minor number then a build number gets incremented each time I compile a...
Hi,I'm runningSTM32CubeIDEVersion: 1.9.0Build: 12015_20220302_0855On Linux and it's started misbehaving while trying to debug while single stepping through code.Ican get one or two steps in and it jumps off to USART3_IRQHandler and won't come back ou...
Does anyone know how to import an IOC file into an existing project?I was trying to have two IOC files; one for issue 1 of the hardware and one for issue 3 and swapping between them, but something's gone funky with it and now the project won't recogn...
I've had a Cube project running for a weeks on a board and it's started behaving really weirdly. It started by crashing when I added a call to read the external SPI ADC. Took it out and it worked. I'd not changed the ADC code so I was bemused by this...
I'm trying to just get a CAN message sent out to prove the hardware on a board. At the moment, the Tx pin is high and even when I attempt to send a message out I get nothing. My first question is:If there is nothing else attached to the CAN bus (post...
Kudos given to