cancel
Showing results for 
Search instead for 
Did you mean: 

internal resistance ADC

Jad
Senior

Good morning. I am working with the Discovery kit with STM32H7B3LI MCU and want to get its internal resistance. I want to use 10 buttons, each with one resistance, and then get the correct value for my MCU. I already know how to get the values between 12000 and 64000. but I do not get what Voltage they describe. I saw on the datasheet of the Chip that it has a linear relation with the voltage and receives a voltage between 1.62 and 3.6V. Still, I have no accurate Information on the internal resistance to calculate my voltage divider. I can do it with the information I have, but I feel like I am missing something. When I put a 120-ohm resistance or shortcut directly to the ADC with 3.3V, it also gives me the maximum value.

Capture d’écran 2025-02-01 à 16.02.36.png

Capture d’écran 2025-02-01 à 16.03.23.png

Capture d’écran 2025-02-01 à 16.03.44.png

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

The convertible input range for the ADC is (0, VREF+) which is typically (0, VDD). It sounds like your board has VREF+ = 3.3V.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Super User

The ADC doesn't have a resistor to ground. You can't use it as one half of a resistor divider. It has some effective series resistances and capacitances.

 

See here for the effective circuit:

TDK_1-1738423739829.png

 

You can do what you're doing, but you will need to use external resistors and have the voltage of the net change based upon what button is being pressed.

If you feel a post has answered your question, please click "Accept as Solution".

ok so i will add a pull down resistance then. Does the value then will go until 3,6V? because i still do not understand why i get the max value when I send 3,3V

TDK
Super User

The convertible input range for the ADC is (0, VREF+) which is typically (0, VDD). It sounds like your board has VREF+ = 3.3V.

If you feel a post has answered your question, please click "Accept as Solution".