STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G474 FDCAN Callback is not called. Classic frame

Hi,I have a custom board with an STM32G474RE. I use 3 CANs with 3 independent CAN tranciever on the board. I tried sendind CAN message from CAN1 to CAN3 but the message is not received. At least the callback funnction is not called. I used an oscillo...

TFegy.1 by Associate
  • 1593 Views
  • 1 replies
  • 0 kudos

I want to print out 5 waveforms in 1us time.

I want to print out 5 waveforms during 1us.So, I printed out 5 MHz period PWM from TIM3.We tried to change the duty cycle of TIM3 to zero at interrupt time by running a 1 MHz timer counter on TIM6. However, it was confirmed that TIM6's 1 MHz timer co...

Jkong.1 by Associate II
  • 2340 Views
  • 4 replies
  • 0 kudos

Resolved! "DMA is not working on STM32H7 devices" article is wrong

I think the article here:https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devicesis wrong. In solution 3 it invalidate D-cache before reception. This doesn't make sense, it has to invalidate the D-cache after reception.

fb by Associate III
  • 4483 Views
  • 3 replies
  • 0 kudos

STM32L010 current consumption higher than expected

Hi,I have a custom board with STM32L010. I used STM32 cubeMX to initialize the GPIO,I2C,SPI,ADC,USART,LPTIM2,CRC,DMA and RTC. Then I de-initialize everything except GPIO and put the controller in sleep mode. The current consumption still is 250 uA af...

ARai by Associate II
  • 5106 Views
  • 8 replies
  • 0 kudos

How to use OSPI with STM32L4R9 on custom board?

Hello,As mentioned in Errata sheet of STM32L4xxx, the auto polling mode is not functional. This mode allows an automatic polling fully managed by hardware on the memory status register. The workout in the Errata sheet is to use memory-mapped mode, bu...

Hzhan.2 by Associate II
  • 1215 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 with SDRAM: How to connect unused DQMs?

Posted on February 12, 2018 at 19:29I'm about to use a STM32F7 MCU with some x16 SDRAM. Since I don't use byte or unaligned accesses, I disabled the NBL pins, which should otherwise be connected to DQMH/L at the SDRAM.But if I don't use those signal...