STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using ADC3 when ADC 1 & 2 are running in DMA

I am successfully using a timer and DMA to capture 4096 samples from ADCs 1 & 2 using a master slave configuration on a STM32H747- Disco board.I would really like to simultaneously capture 3 channels. Is it possible to capture samples from ADC 3 usin...

AStew.1 by Associate II
  • 828 Views
  • 0 replies
  • 0 kudos

Stm32H7 DMA ADC Low Bit Resolution

Hello Everyone,I am using the stm32h7 to sample 4 channels from adc1 using the DMA.I am using circular mode with half word size. I start the dma and let it fill up a memory buffer:volatile uint16_t adcInsDMA[4*ADCBLOCKSIZE] = {0};   HAL_StatusTypeDe...

0693W000008y4RNQAY.png
TCash.1 by Associate III
  • 1741 Views
  • 5 replies
  • 0 kudos

Resolved! Blinking LED

Hi all,Just started with bare metal programming of stm32f411re.Uploaded the following code to blink the onboard led of the nucleo board.Code:#include "stm32f4xx.h"         // Device headervoid delayMs(int delay);int main (void){RCC->AHB1ENR |= 1;GPIO...

KRaja.1 by Associate
  • 1834 Views
  • 2 replies
  • 0 kudos

Connecting STM32F7 FMC with SDRAM and 8 bit data bus

When using a 16 bit data bus, the STM32CubeMX generates outputs for FMC_NBL1 and FMC_NBL0 that connect to the SDRAM DQMH and DQML pins. If the STM32CubeMX is configured for an 8 bit data bus, there is no DQM pin generated, although the 8 bit SDRAM h...

MPatt.11 by Associate II
  • 4998 Views
  • 6 replies
  • 0 kudos

STM32H750VB

Hello,I want to ask if it is possible to drive TFT with FMC (Flexible Memory Controller), our TFT has only MCU interfaceI think EMwin has no option for MCU interface at STemWin_CM7_wc16 library.We used same TFT with STM32F207 by using FSMC .If its n...

AKINI by Associate III
  • 834 Views
  • 0 replies
  • 0 kudos

How to implement SM bus restart condition for implementing Smbus block read protocol on master side and how will the slave respond?

Which Xferoption should be selected and should we use both functions ieHAL_StatusTypeDef HAL_SMBUS_Master_Transmit_IT(SMBUS_HandleTypeDef *hsmbus, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t XferOptions)andHAL_StatusTypeDef HAL_SMBUS...

0693W000008yg7kQAA.png
VKamb.1 by Associate
  • 1181 Views
  • 0 replies
  • 1 kudos

Resolved! Generating specified number of pulses using PWM

Hi All,I am trying to generate required no of pulses using PWM. This is to implement to control stepper motor with position control. I use HAL_TIM_PWM_Start_IT to start pulsing and count the no of pulses in HAL_TIM_PWM_PulseFinishedCallback. I notice...

0693W000008ye9AQAQ.png 0693W000008ye95QAA.png 0693W000008ye90QAA.png 0693W000008ye8vQAA.png
Ayemyitta by Associate II
  • 9180 Views
  • 12 replies
  • 0 kudos

Resolved! Synced timers with period multiples

Hey folks!Got some questions around synced timers on STM32F401, where the aim is to have two timers start together, where one timer has a period an integer multiple of the other. I've got what I need working but how it works, doesn't add up.Here's th...

0693W000008yfGMQAY.png 0693W000008yfGHQAY.png
DCall.1 by Associate
  • 1769 Views
  • 3 replies
  • 0 kudos

Resolved! ARM Cortex M4 assembly questions

Hello everyone,I'm just starting to learn assembly for the ARM architecture. I'm also in general a beginner with the assembly language I have just some minor experience with the x86 assembly but that's about it.I'm following a course on Udemy and I h...

PPopo by Senior
  • 3383 Views
  • 3 replies
  • 0 kudos