cancel
Showing results for 
Search instead for 
Did you mean: 

MCU with 13 bit ADC.

JJeon.2
Associate II

Hello.

Please make a product with 13 bit ADC.

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Uwe Bonnes
Chief

Oversample with a 12-bit ADC or use the 16-bit ADC of H7.

Or STM32F373 ... are you sure that you looking for 13bit ADC ?

Thank You.

stm32F373=MCU with 16bit adc​

A 13-bit or 14-bit product is sufficient.

Thank You.​

Uwe Bonnes
Chief

Look at the "EG" specs of the SDADC in the F37x in table 74. If you need accuracy, I think the SDADC in the F37 is nearly useless!

Good point. May be it can be corrected by manual gain calibration. But also linearity error looks poor. Definitely better use external ADC if looks for accuarcy ...

Uwe Bonnes
Chief

Or oversample internal ADC.