User Activity

Will IC such as L6924U operate with AC ripple on the power input? That is as if the power input were rectified AC with no reservoir capacitor?I posted this before but can not find the post now? Sorry for duplicating the question if it is duplicated...
Will all or any battery charger ICs such as L6924U operate properly with rectified AC input?The rough circuit below is of a bicycle dynamo that delivers 300mA-500mA of varying AC frequency and current ripple will this prevent the charger controller f...
I would like to use a SMP controller such as L6726 or other as a boost regulator. That is use the high side output (pin PHASE) connected to 0V and my boost transistor. I would use the low side driver to drive a MOSFET as a synchronous rectifier Is ...
Can either A6727 or L6726A buck controllers be used as a boost controllers by connected the high side driver (Phase) to 0V to drive my power transistor?Alternatively do you have spice models that I could use on LTspice or Tina-TI for example. Please ...
Microcontroller may be; STM32L0 or L4Required; 5% worst case over -5 to 50'C​The microcontrollers are quoted 1% accurate at 25'C but I can not find how accurate they over the ICs temperature range. I want to avoid trimming or fitting a crystal.​​The ...