STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FMC NAND Timing Issue

Hi,I took reference  for calulating the timing / cycles for my MT29F1280AJAAA (I'm using STM32H745ZIT3) In Asynchronous mode - 5, which is saying ~50Mhz in the datasheet. But I'm running FMC at 131MHz clcok, what ever the calculation I have calculate...

Lucifer37 by Associate III
  • 232 Views
  • 1 replies
  • 0 kudos

STM32, DAC output buffer, maximum safe output current

Hello,I want to know the DAC output buffer maximum safe output current before damaging the output buffer. I know that it's not possible to get the output swing mentioned in the datasheet under this condition.The datasheet maximum ratings doesn't stat...

RAltm by Senior
  • 455 Views
  • 7 replies
  • 0 kudos

Resolved! Connection of Power and XSPI

Hi,This is my first time using an STM32N6 without internal flash, and since I am right before handing over files for artwork, I would appreciate it if you could check if the power lines and XSPI memory connections are correct.I have searched around a...

pic1.png pic2.png

Resolved! Problem to set FDCAN2 in STM32CubeMX for STM32H562RGT6

Hello,I am planning to use STM32H562RGT6 in my product to communicate and update my firmware via CAN FD.To plan that, I am using STM32CubeMX 6.17.0, the datasheet and the AN2606 (Rev 70).And I would like to use only one CAN FD to communicate and to u...

x314159_1-1776260323976.png x314159_2-1776260360172.png x314159_3-1776260415863.png
x314159 by Associate
  • 295 Views
  • 3 replies
  • 2 kudos

Resolved! Wrong voltage typed at Vrefint STM32C092

I have followed the datasheets and tried to calculate my reference voltage. I am supplying steady 3V on Vref+ pin but I wanted to confirm this because I have some troubles with the ADC precision.So I read the internal voltage both on my card and on a...

morris_0-1776092976724.png Skärmbild 2026-04-13 153204.png
morris by Associate III
  • 278 Views
  • 3 replies
  • 1 kudos

Need help in erasing the device: STM32H735IGK3

HiI need help in erasing the device: STM32H735IGK3, This device is getting erased only till sector 0.There were total 8 sectors.I am following the steps given in  Reference manual for erase operation but still it didn't work.Could you please suggest ...

Saista by Associate
  • 184 Views
  • 2 replies
  • 0 kudos