STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RDP Protection

Hi I'm using STM32F411RET6 MCU. I tried to connect using the programmer to download the firmware, but there was an error as shown below, and the data cannot be read. 13:18:34 : UR connection mode is defined with the HWrst reset mode13:18:34 : ST-LINK...

giwonKIM_0-1755663629237.png
giwonKIM by Associate III
  • 1176 Views
  • 6 replies
  • 0 kudos

Resolved! STM32U3: 3V3 tolerant GPIO at 1V8 supply ?

Hi, I am using STM32U385CGU6 with 1.8V supply. My GSM peripheral using the 3.3V Uart port for a dedicated time (2sec) then turn back to 1.8V level of UART.  Could you offer 3.3V tolerant pin? I am using PA8 to communicate with GSM module. thank you &...

FERAMUZ by Associate
  • 288 Views
  • 3 replies
  • 2 kudos

Resolved! L0 I2C slave RX DMA - clean cancel with I2C STOP ?

Heyho,using L073 at 32MHz, so even I2C transfers "seem" fast, at least in "fast mode plus" at SCL 1 MHz. And I don't want to over-use clock stretching.I'm looking for a way to use I2C slave receive with DMA, but an unknown transfer length.Right now i...

LCE by Principal II
  • 182 Views
  • 1 replies
  • 0 kudos

STM32L1 NRND'd

One of my friends noticed, that ST NRND'd not only the STM8, but also the whole STM32L1xx family.However, in contrast to STM8, the 'L1 are under the 10-year commitment program, so they should continue to be available in the next 9 years. JW

0693W00000YAFcGQAX.png

STM32H75x QSPI flash memory mapped mode questions

Hi,I've have to port an existing huge application from F4 to a H753 board. The F4 has PNOR the H7 dual QSPI flash.One task parses XML configuration data from PNOR flash. A second task stores data e.g. log data in same PNOR.Parsing configuration data ...

regjoe by Senior II
  • 461 Views
  • 7 replies
  • 3 kudos