STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H753I-EVAL2 touch screen functionality

Is there any sample project that can guide in configuring touch screen functionality on the VGA LCD in STM32H753I-EVAL2 board. As of now, I have not found any relevant documentation regarding the same.

hrm2519 by Associate II
  • 1404 Views
  • 2 replies
  • 0 kudos

How to program using VIM + GCC on STM32F415?

Hi, I'm a complete noob, coming from Arduino (MCU: ATmega328p) Board and I want to have similar programming environment there.General information:OS: LinuxMCU: STM32F415Board: custom one which has USB Mini B portI would like to use GCC + VIM if possi...

0xZER0 by Associate II
  • 4345 Views
  • 3 replies
  • 1 kudos

stm32h750 qspi bank 2 only

Can I use a external flash in qspi mode connected to qspi peripheral bank 2 ?I wan to test 2 things:Dump code from ext flash to sram partition to execute appExecute in place code in ext flash I use bank2 because in lqfp 100 package i had direct and c...

JCuna.1 by Senior
  • 909 Views
  • 1 replies
  • 0 kudos

Lossless data processing

Hello,I'm working with STM32F410RB , My question is not related to code but it's architectural. I'm using DMA uart to communicate with another device, i noticed that dma buffer change its content before my code processing the data. So i'm loosing som...

Ahajr.1 by Associate II
  • 1633 Views
  • 2 replies
  • 0 kudos

SPI Mode get change in execution it get stuck

I am working on Nucleo-h745ziq board .I have to board i am doin the loop-backing. One board as master and another as slave. First I configure as both board as full duplex. After switching the switch the mode get change the MASTER only transmit and s...

MDeva.1 by Associate II
  • 943 Views
  • 1 replies
  • 0 kudos

Resolved! When cache is enable DMA not update data

I am working on Nucleo-h745ziq board .I am enable the ADC ch3 and 12 bit resolution ,DMA is enabled and circular mode. I connect the 3v supply to ADC channel. But I doesn't get the updated value when I reset board I get updated value, when I disable ...

MDeva.1 by Associate II
  • 1802 Views
  • 3 replies
  • 0 kudos

STM32H753i-EVAL2 LCD functionality

I am using the STM32H753i-EVAL2 board to test LCD and touch screen functionality. Currently I am unable to generate the code using CubeMX as sample codes dont have the .IOC file. I need help in setting up the LCD and touch screen via CubeMX.It is dif...

hrm2519 by Associate II
  • 2211 Views
  • 4 replies
  • 0 kudos