cancel
Showing results for 
Search instead for 
Did you mean: 

With CR_BYPSHAD=1 on STM32L4R5xx, is the RTC (RTCv2) SSR counter reset to RTC_PRER_PREDIV_S when calendar time is updated (HAL_RTC_SetTime)?

FLott.1
Associate

My testing appears to consistently show that whenever I update the calendar time and date, the RTC_SSR I read straight after the set operation is the RTC_PRER_PREDIV_S value.

However, I fail to find this explicitly stated anywhere? Maybe its obvious, but I need to know if I could rely on this.

(1) Is the RTC_SSR (direct mode - not shadow) reset when exiting INIT mode?

(2) RTC examples update date and time sequentially, explicitly exiting INIT mode between HAL_RTC_SetTime and HAL_RTC_SetDate. Is this safe? Does it rely on the fact that INIT mode exit takes 4 RTC CLK ticket to start counting?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User
  1. Yes. This is documented in Calendar initialization and configuration subchapter, although not in the clearest way.
  2. Cube/HAL is not famous for being brilliant. Nonetheless, it takes one second for the subsecond counter to underflow.

JW

FLott.1
Associate

Understood, thank you. In summary, Setting time first resets the SSR, which means you will less likely end up on a second edge between setting the time and date (assuming no RTOS task scheduling / interrupt interference).

However with all the external factors mentioned, it is probably best updating time in a way that prevents interference (maybe scheduling the update on a high priority RTC second interrupt). I have a PPS edge (PC13 pin) I use with the Timestamp feature to correct the second edges, and GNSS time source which will regularly update the time / date.

Thanks for your quick feedback.

waclawek.jan
Super User

> it is probably best updating time in a way that prevents interference (maybe scheduling the update on a high priority RTC second interrupt).

Or just simply don't use the Cube/HAL functions, write your own.

JW