Skip to main content
AKayd.1
Visitor II
May 8, 2021
Question

Synchronous converter phase shift between PWM signals

  • May 8, 2021
  • 1 reply
  • 881 views

I am designing a 4-phase interleaved synchronous boost converter. Each phase has 2 MOSFET's which are not to be in conduction at the same time. I'm using STM32F407 discovery board. I am making use of TIM1 AND TIM8 channels to get complementary PWM's which ensures deadtime between two same-phase signals.

The problem is that I couldn't figure out a way to create a phase shift between the channels of TIM1. This would yield at least 2 pairs of pwm signals with their complementaries which are 90 degrees phase shifted and I could get other 2 pairs from TIM8. Creating the phase phase shift between two timers (like TIM1 and TIM2) is not an issue when using CNT registers.

I am not a very experienced user, comments and suggestions are very much appreciated, thanks!

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
May 8, 2021

> The problem is that I couldn't figure out a way to create a phase shift between the channels of TIM1.

You can't.

In newer STM32 models, there is a Combined mode which would allow you that, but not in 'F4.

JW