STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Minimum pulse width for STM32F2 timer in input capture mode.

I have a low frequency (~1 kHz), low duty cycle signal that I'd like to capture rising edges of. What's the minimum width of those pulses to capture them using a timer in input capture mode?I see there's a programmable digital filter there, in terms...

RGadd.2 by Associate
  • 1697 Views
  • 2 replies
  • 0 kudos

Resolved! Why is does the ADC stay on 2048 (12Bit)?

Hello Our STM32G4 is measuring a sinus-ADC value with offset. The offset is at VDDA/2.Our ADC measurement shows a plateau at the offset, even, when the sinus signal is crossing the VDDA/2 (see attached picture).The signal them self seems to be ok (me...

RGmün.1 by Associate II
  • 7422 Views
  • 8 replies
  • 0 kudos

How reinit UART?

After reset MCU init UART - 8bits, no parity bit, init DMA RX and TX, interrupts on - works Ok.Reinit UART - 9 bits, even parity bit, no DMA - works Ok.Reinit UART the same as p.1 - doesn't work interrupts.

EAlek.2 by Associate II
  • 3994 Views
  • 3 replies
  • 0 kudos

Gimbal 3-axis with STM32 and MPU6050

Hi I have been thinking about making a 3 axis gimbal with Arduino and an MPU6050 for some time now. I went around the internet for a while and saw that there is a project that manages to control three brushless motors only with arduino as if they wer...

SCasa.2 by Associate
  • 3183 Views
  • 2 replies
  • 0 kudos

Nuclel STM32F303K8 TIM2 as Encoder

I'm working to read 2 identical encoders from 2 identical motor drivers.I use TIM2 and TIM3 to read the encoders.The encoder at TIM3 works properly, but the encoders at TIM2, I could see in debug mode the IRQ but the register CNT is zero. But every t...

FTrom by Associate II
  • 1582 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H745 SDMMC DMA Rx Overrun/Tx Underrun

Hi,I am working on STM32H745 discovery board and trying to configure the onboard 4GB eMMC flash over SDHC1 interface. I am loading default discovery board configuration by the CubeMx configuration, which sets both M7 and M4 and all AHB buses to run a...

Joyabb by Associate II
  • 3930 Views
  • 3 replies
  • 0 kudos

how to protect analog inputs ?

I've seen the discussion in an old question herehttps://community.st.com/s/question/0D50X00009XkbAd/how-to-protect-analog-inputs-Accordingly, ADC inputs are not 5v tolerant in ADC mode.I started studying some Zener diodes, in particular 1n4727 Vz 3vh...

andrewg by Associate III
  • 3764 Views
  • 4 replies
  • 0 kudos