STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 watchdog does not correctly reset. Example attached

I have been battling an issue for a while where upon a watchdog (WWDG1) timeout, the system was not correctly reset. I was finding that the CPU and NVIC are reset but all the peripherals are not reset after a watchdog reset, they keep their exact reg...

0693W000000WsqyQAC.jpg 0693W000000WsrDQAS.jpg 0693W000000WsrSQAS.png 0693W000000WssVQAS.png
ADunc.1 by Senior II
  • 15080 Views
  • 34 replies
  • 5 kudos

STM32H743 3ADC's With DMA

I have implemented 3 ADC with DMA. ADC1 with DMA1 stream 0 , ADC2 with DMA2 stream 0 and ADC3 with BDMA channel 0 Resolution : 16 bit , ADC clock : 7MHZ , Sample : 8.5 cyclesAll these ADC are Time trigger for that i am using timer 1 as center aligned...

Kanna by Associate III
  • 3565 Views
  • 8 replies
  • 0 kudos

STM32 Nucleo I2C Slave answer with Interrupt

Hello, everyoneI'm trying to make an I2C slave with a Nucleo-F401RE.Writing from Master (Raspberry) to Slave (Nucleo) works very well.But the response of the Slave (Nucleo) to a read command from the master (Raspberry) does not work.I tried a very si...

0693W00000DlqjxQAB.png 0693W00000DlqlKQAR.jpg
SBühl.1 by Associate
  • 1357 Views
  • 1 replies
  • 0 kudos

Resolved! Wake-up from RTC-alarm works only once

I am trying to set RTC-alarm event to wake up an STM32F103C8T6 from sleep-mode (not standby, not stop) and it works once, but subsequent alarms never wake the MCU up. Nothing I've tried seems to work and I no longer have any idea how to fix this.The ...

Is it possible to use analog watchdog without adc interrupt?

I am thinking of turning on ADC with DMA when analog watchdog detect certain level of signal. Then I would like to turn on ADC with only watchdog first and when LevelOutOfWindowCallback() is called ADC with DMA starts. I tried code below but it didn'...

SShir.2 by Associate II
  • 1695 Views
  • 2 replies
  • 0 kudos

Resolved! Trouble with multiple ADCs and DMA

I'm trying to get ADC values from multiple channels of ADC1 of STM32F103C8T6 using DMA where conversion is triggered by TIM3 every 1ms. However, I'm not seeing the right values. I tried the polling mode and that worked fine. Here is the main function...

0693W00000DmDkyQAF.png 0693W00000DmDlDQAV.png 0693W00000DmDlIQAV.png

remarks about ST quality of education

Hello,My goal is to evaluate several ARM Cortex-M4F chip manufactures and select the one that best fits my needs for building IoT devices. I will admit that I am on the learning curve and that I’m doing this on my spare time. I’ve read a lot of books...

gdori.1 by Associate II
  • 2385 Views
  • 5 replies
  • 1 kudos