STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Any option to go with STM32H745ZIT3 in VOS0 and VOS1 mode to use the maximum clock frequency in the industrial temperature Range variant.

Due to the current semiconductor shortage the microcontroller STM32H745ZIT6 is not available in the quantity of 210, so I had to buy the variant with higher temperature range. However, the data sheet says in small print that this variant does not sup...

SMein.1 by Associate II
  • 1337 Views
  • 2 replies
  • 0 kudos

Custom SPI Datasize

Hello, I am trying to interface to an external ADC via SPI. I amusing the STM32Cube IDE with a Nucleo-144 STM32L552. The issue I am having is that the ADC requires an unusual number of clock pulses (18 as per data sheet - see attached screenshot). No...

SJohn.5 by Associate II
  • 4772 Views
  • 3 replies
  • 0 kudos

STM32F4 using DMA2 for USART1

I am using a STM32F407, and I would like to use DMA to receive data from USART1 and store in a buffer.HAL is not being used.USART1 is configured and is receiving the first byte of the message correctly. That is, the data shows up in USART1->DR.Here i...

0693W00000HnYbgQAF.jpg 0693W00000HnYbqQAF.jpg
gahelton1 by Associate III
  • 4608 Views
  • 6 replies
  • 0 kudos

Resolved! How to solve "undefined reference" when compiling

I took the driver from Arduino for ADS119X and implement the HAL code for STM.When compiling, it gives me “undefined reference to `keepSetting'�?. First I tought on a code problem but after long time of trail and error, I was looking on forums. It’s ...

Using "HAL_CAN_AddTxMessage" from interrupt and main loop

Hi, I want to be able to add CAN message with "HAL_CAN_AddTxMessage" from interrupt and main loop (loop maybe busy sometimes so I cant send all messages from it). I assume they can collide and override so its not safe to do it from both?What are my o...

JBond.1 by Senior
  • 899 Views
  • 0 replies
  • 0 kudos