STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The difference between VREF+ and VDDA of STM32F407

Is the following note quoted from the specification of STM32F407 applied to all the time from power-up or just during the period when the analog data is being sampled?「4. If VREF+ pin is present, it must respect the following condition: VDDA-VREF+ < ...

捷鄭.1 by Associate
  • 1679 Views
  • 2 replies
  • 1 kudos

I need to transmit two buffer trought HAL_UART_Transimit_DMA. I wrote in the code two consecutive command to do it but when I run the code, HAL_UART_Transimit_DMA do not return HAL_OK. It return HAL_OK only in debug mode stepping with F6. Why?

uint8_t slv_add[] = {0xF1, 0x0A, 0x00, 0x57, 0x53};                            if(HAL_UART_Transmit_DMA(&huart1, &slv_add, (sizeof(slv_add)/sizeof((slv_add)))) != HAL_OK)Error_Handler();uint8_t cell_sel[] = {0x91, 0x00, 0x0D, 0x06, 0xA8, 0x6E};      ...

GMart.6 by Associate II
  • 1451 Views
  • 2 replies
  • 0 kudos

Resolved! i2c to communicate two STM32F103C8T6

hello,i am trying i2c to communicate two stm32f103c8t6 . It is not working. logic analyzer output is shown in picture.what can be done for i2c to communicate two stm32f103c8t6 address 0x00

0693W00000HoeKxQAJ.png
SSaya.1 by Associate II
  • 2200 Views
  • 3 replies
  • 0 kudos

MFI SDK for STM32

Is there a software addon, SDK or examples for the apple MFI program for STM32 available?We are already MFI members.Thanks,Gabriel

GFell.1 by Associate II
  • 1075 Views
  • 0 replies
  • 0 kudos

Why toggling of Port E inside the timer 2 interrupt handler only work if the APB1 prescaler is set to /2 or /4 only?

I have a Timer 2 interrupt handler  which will toggle the Port E output. My MCU is STM32F407 running at 168 Mhz. I found that the toggle code inside the interrupt handler only work if the APB1 prescaler is set to /2 or /4 only. Slower ABB1 frequency...

nNg.1 by Associate II
  • 2328 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F10x Flash size mismatch

I have a bunch of Blue Pill boards I'm re-animating (ye olde chippe shortage, y'know). Attacking them with stm32flash reports a flash size of 128 kBytes. On the other hand, 0x1FFFF7E0 contains 0x40, indicating 64 kBytes of flash.Now, which of these i...

B-U585: Qualify SSID with space: Not good!

Hello,the B-U585 Demo when asking for the SSID qualifies a name with a spacebar. Problem is, that many SSIDs contain a space by itself, like "FRITZ!Box 7530 ..." or "Galaxy ...". As the application does not echo what is sees, useres are left in the d...