STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is written to the USART_BRR register?

What is this value that is written to the USART_BRR register?What is it for?I don’t understand why the calculation is done using the formula: fclock / (the divisor, in my formula it is 5 * baudrate)For example, here is an example calculation:I made t...

0693W00000NskeHQAR.png
MMust.5 by Senior II
  • 9911 Views
  • 18 replies
  • 0 kudos

STM32F405 SD DMA only works once, no matter what

Hello,I am currently trying to get an Adafruit Feather STM32F405 board to write to files on an SD card using DMA. I'm using CubeIDE, not STM32duino, and I have tried DMA configurations with both a single stream and two streams (one RX and one TX). No...

0693W00000NsdEHQAZ.png
liamur by Associate II
  • 2170 Views
  • 3 replies
  • 0 kudos

STM32H743 PWM

hello friends)))) I bought a new stm32H743 for familiarization and got confused how to implement PWM on HRTIM. I'm trying to do PWM on timer B. configured GPIO_PC8 to AF1 in GPIOx_AFRH. everything is fine there.HRTIM_B_PERxR==2000 HRTIM_B_CMP1xR==200...

MTS by Associate II
  • 2700 Views
  • 6 replies
  • 0 kudos

Firmware Behaviour change after files clean up

I am working on a state machine to control a stm32f334 mcu, first state would be general initialization, the wifi initialization, waiting for stable input and some other states that are not relevant here. It was working smoothly and I wanted to commi...

ISust.1 by Associate
  • 840 Views
  • 0 replies
  • 0 kudos

STM32G491 (Flash category 4): Flash IAP programming?

Hi, I would like to re-program only some higher part of flash memory with In-Application-Programming (Chip: STM32G491 - this in RefMan is defined as "Flash category 4" device).My normal firmware e. g. is running in lower 256kB Flash.And now I want to...

flyer31 by Senior
  • 1037 Views
  • 1 replies
  • 0 kudos

STM32F439ZI first embedded flash program issue

Hi,I'm working with STM32F439ZI MCU. I setted system clock 180 MHz and as Reference Manual (RM0090) says I did:-- VOS[1:0] = 0x11-- over drive mode enabling-- 5 WS latency (6 CPU cycles)When I try to program something the first time after power up, i...

AFara.2 by Associate II
  • 1821 Views
  • 3 replies
  • 0 kudos

Resolved! MCU type - Can one identify it?

Using something like STLink util or newer, command line software: Can one identify which type of STM32 MCU is connected? E.g. for use in further scripts. It doesn't help if I see it on a GUI somewhere.